STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have ported X-CUBE-SBSFU to my own board successfully and can update the firmware via the UART, but am now looking to update in app from a web server similar to how it is done is the X-CUBE_GCPv2.

I actually have not tried it out yet, but looking at the code, I think the SBSFU in the X-Cube-GCP package is not the same as there are some things that are very different (like the slot names for example)Need some advice from the ST reps hereWould ...

Eugene G by Associate III
  • 1300 Views
  • 1 replies
  • 0 kudos

Critical failure SBSFU during firmware update

======================================================================                                                                 =             (C) COPYRIGHT 2017 STMicroelectronics                =                                               ...

OAber by Associate II
  • 1392 Views
  • 1 replies
  • 0 kudos

SBSFU on Dual Core STM32 Microcontrollers

Hi could I find out if anyone has successfully got X-CUBE-SBSFU running on the dual core components? There does not seem to be any examples from ST for these use cases.The dual core components I am aware of are H745/755, and H747/757. However all of...

DN_1 by Associate II
  • 1651 Views
  • 2 replies
  • 0 kudos

About the Entropy Health test function

Hi AllI need to fill the security policy about STM32 crypto library(STM32CubeExpansion_Crypto_V3.1.0), and had three function name to fill.1, Entropy Health test2, Repetition Count Test3, Adaptative Proportion TestAnyone knows these?Regards,

YChen.51 by Associate II
  • 886 Views
  • 0 replies
  • 0 kudos

Unable to port STM32F413H-Discovery 2_images to STM32F417

I'm sure I'm missing out something obvious as I'm fairly green with limited programming experience, but I could not port the STM32F413 project to run on my own STM32F417 board. I've scoured this topic and followed Security Part6 - STM32 security ecos...

Eugene G by Associate III
  • 1623 Views
  • 2 replies
  • 0 kudos

Can't seem to get correct results from CRC hardware

I have a routine that I have used for years on other processors and on PCs to get a CRC16 X-25 from a string. I'd like to get the hardware CRC to use the same CRC16.I have tried every variant in the STM32CubeIDE and have not been able to get same out...

JimFouch by Associate III
  • 3474 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.