STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hello, I'm using an STM32H750 MCU where I'm integrating the Crypto lib v4.0.1 I would like to execute this library (.text) from a specifc section. But I can manage to do what I want.

You can found below a extract of my linker script:MEMORY { D1_CODE_RAM (xrx) : ORIGIN = 0x24070000, LENGTH = 64K FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 128K NVRAM (rx) : ORIGIN = 0x8020000, LENGTH = 64K }   .ram_code_load...

DFell.1 by Associate II
  • 1469 Views
  • 1 replies
  • 0 kudos

STM32WB5x IEEE 802.15.4 Stack

Hey, I'm Working with STM32WB5x on a bare metal MAC 802.15.4 Application.I Have the BLE_MAC_***_FW latest (version 1.13.0) installed on CM0+ .I want to add security for MAC Frames with support for both ENC-MIC. The current ST WPAN MAC 802.15.4 implem...

MYous.3 by Associate II
  • 1718 Views
  • 1 replies
  • 0 kudos

SBSFU Firewall reset in User App when writing to SFR's.

Hi All,I am almost finished integrating the SBSFU into my project. I can run the SBSFU and user app and update the processor, STM32L4R9VITx, successfully while no protections are enabled. When I enable firewall protection it boots into my application...

0693W00000LvolKQAR.png 0693W00000LvoltQAB.png
RBurg.2 by Associate II
  • 5337 Views
  • 11 replies
  • 0 kudos

Resolved! Inconsistency between STM32H7 AES HAL and Reference Manual

HelloI'm starting to implement AES-GCM on STM32H753 (rev V).I've found an inconsistency between the HAL and the Ref Manual.The STMicro HAL for AES for STM32H7x3 is setting some bits called NPBLB in CRYP_CR register if the product revision is above re...

Gpeti by Senior II
  • 3729 Views
  • 7 replies
  • 0 kudos

Resolved! Unable to install X-CUBE-SBSFU on STM32CubeIDE

I received today the link to download version 2.6.0 of X-CUBE-SBSFU. Is it possible to install it along with the other X-CUBE Packages within the STM32CubeIDE? I successfully verified the integrity of the downloaded file and tried to install it using...

0693W00000LxBeYQAV.png
ntestoni by Associate
  • 1698 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.