2021-12-03 1:22 AM
2021-12-15 4:14 AM
@Community member "Have you actually used it?"
Not the LVGL one, but the others I mentioned.
"it's just another javascriptoid facebook-ish disaster"
That's not what I see on the ones I've used. Maybe it's configurable?
large whitespace - OK, maybe that one.
"suggested topics" automagic - is actually quite useful: I find it quite often does turn up relevant existing threads.
But, again, the way it guides new users through how to use the forum is a key feature - as @Community member said, "There should be some sort of page which describes how to ask a good question that we can point these low-effort posts to"
2021-12-15 4:17 AM
@Community member - "There should be some sort of page which describes how to ask a good question that we can point these low-effort posts to"
Better yet, something that is presented to new users before they get to make their first post.
2021-12-15 4:55 AM
Hi @Community member
I hear you loud and clear about your expectations for the community, no doubt about that, and I agree that our internal systems should never get in the way of the usability of the community. We are working towards that, I guarantee, but I have to be realistic and say that you will probably not see major changes to the structure of the community and its systems in the next couple months.
To your points:
Thank you!
2021-12-15 5:22 AM
Make the scoreboard and ranks to use and maybe show the forum differently for a newbee from veteran ?
2021-12-15 5:23 AM
eevblog looks like Arduino for STM32 - Index page (stm32duino.com) ?
2021-12-15 6:06 AM
I've noticed another functional improvement: you can now paste an image directly into a post!
:grinning_face: :thumbs_up:
Although it does give a rather cryptic pop-up when you do that:
Given the troubles some users seem to have with basic computer/web literacy, I'm not sure what they're going to make of that...
:\
2021-12-15 6:12 AM
> Maybe it's configurable?
It undoubtedly is.
I also tried to switch off javascript, and to my utter surprise, Discourse kept at least displaying messages in a sane - and arguably better - way.
> guides new users
Maybe. But don't hold your breath; these users behave in this way not because they did not receive some guidlines, but because it's a deeply rooted and long-lasting cultural thing.
JW
PS. I'm glad we make this mess here, highlighing both the idiocy of paging and the need for flat display of thread.
2021-12-15 6:52 AM
I agree that there should be register level examples for most things, certainly for timers, uart, SPI, etc. Probably not for USB. They implemented the idea zone, that idea was BY FAR the most highly rated idea, and yet it's been dismissed. Shrug.
But apart from that, I think HAL is a large improvement over SPL. Rather unfortunately, LL is a giant leap backwards but it's easy to ignore it.
If we take STM32CubeIDE separate from the code generation in STM32CubeMX, I think most of the debugging features, fault analyzer, memory usage tools, peripheral register viewing, have been improvements. I like CubeMX for the pin layout and clock visualization, but not as much for the code generation.
2021-12-15 6:52 AM
This rare fix predates this update, I've even praised it somewhere, can't find now that post.
[EDIT] found it [/EDIT]
JW
2021-12-15 7:15 AM
> limit of 8 topics per page
I mean that, without scrolling, you can only see 8 topics per page. I think it should be more like 20, which would allow you to scan topics easier. Info could be compressed here to make better use of the vertical space. Although I did look at other forums and was surprised that the average posts per vertical page is about 12-15. ST was still the worst, but not a huge outlier.
> Knowledgebase
Hmm, did this change in the past 2 weeks? The current layout looks good. I retract my comment about that. I remember it showing only 6 posts per topic and needing to click on "show all" or something.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.