2015-06-23 8:36 AM
Dear community,
I try to use the NUCLEO F302R8T6 board which I initialized using a start-up.c – file which was generatedby the STM32F30x_Clock_Configuration_V1.0.0.xls tool. I changed the NUCLEO board configuration accordingly to the UM1724 User manual for STM32 Nucleo boards page 22 5.7.1 -> MCO from STLINK to use the 8 MHZ produced by the on board quartz. The system_stm32f30x.c file (which I renamed into “system_stm32f3xx.c�? to make it compatible with the KEIL CMISS package) contains the following definition:
//Definition
*=============================================================================
* Supported STM32F30x device
*-----------------------------------------------------------------------------
* System Clock source | HSE
*-----------------------------------------------------------------------------
* SYSCLK(Hz) | 8000000
*-----------------------------------------------------------------------------
* HCLK(Hz) | 72000000
*-----------------------------------------------------------------------------
* AHB Prescaler | 1
*-----------------------------------------------------------------------------
* APB2 Prescaler | 1
*-----------------------------------------------------------------------------
* APB1 Prescaler | 2
*-----------------------------------------------------------------------------
* HSE Frequency(Hz) | 8000000
*----------------------------------------------------------------------------
* PLLMUL | 2
*-----------------------------------------------------------------------------
* PREDIV | 2
*-----------------------------------------------------------------------------
* USB Clock | DISABLE
*-----------------------------------------------------------------------------
* Flash Latency(WS) | 2
*-----------------------------------------------------------------------------
* Prefetch Buffer | OFF
*-----------------------------------------------------------------------------
*=============================================================================
I initialized the USART using the following routine:
void COM_USART1_Init() { //COM_TypeDef COM, USART_InitTypeDef* USART_InitStruct)
GPIO_InitTypeDef GPIO_InitStructure1; //GPIO STruct
GPIO_InitTypeDef GPIO_InitStructure2; //GPIO STruct
USART_InitTypeDef USART_InitStructure; //USART Struct
NVIC_InitTypeDef NVIC_InitStructure; //for USART
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); //GPIOA_AHBPeriph_CLOCK
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); //ENABLE USART3 CLK
// Configure the GPIO_struct USART Tx as alternate function push-pull
//PA10 ->RX
//PA9 ->TX
GPIO_InitStructure1.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure1.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure1.GPIO_OType = GPIO_OType_PP; //PushPull (Gegentakt)
GPIO_InitStructure1.GPIO_PuPd = GPIO_PuPd_UP; //NO Pull
GPIO_InitStructure1.GPIO_Speed = GPIO_Speed_50MHz;
// Configure the GPIO_struct USART Rx as alternate function push-pull
GPIO_InitStructure2.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure2.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure2.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure2.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure2.GPIO_Speed = GPIO_Speed_50MHz;
//Init GpioStruct
GPIO_Init(GPIOA, &GPIO_InitStructure1);
GPIO_Init(GPIOA, &GPIO_InitStructure2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_7); //Connect the PINS and USART BUS
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_7);
//NVIC for USARR
// Enable the USARTx Interrupt
NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; // one level lower than TIm !!
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
// USART 1
// USARTx configured as follow:
// - BaudRate = 115200 baud
// - Word Length = 8 Bits
// - One Stop Bit
// - No parity
// - Hardware flow control disabled (RTS and CTS signals)
// - Receive and transmit enabled
USART_InitStructure.USART_BaudRate = 115200;//9600;//115200; //is just the half of 115200 57600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
// USART configuration
USART_Init(USART1, &USART_InitStructure);
// Enable USART
USART_Cmd(USART1, ENABLE);
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable the USART1- receive interrupt
}
Accordingly to CLIVE1’s post I set the HSE_VALUE to 8000000
(
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/wrong%20usart%20baudrate%20after%20change%20of%20crystal&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=89
)
However the baud rate of the USART is twice as fast as defined (to get the desired baud rate I have to initialize the USART using 0.5* desired baudrate).
I would be very happy if someone could point me into the right direction how to set the clock speed of the cpu correctly.
2015-06-23 9:27 AM
Your PREMUL/PREDIV seems to be non-sense for getting an 8 MHz clock to 72 MHz, review some actual examples in the library, and don't use the Excel sheet/tool.
You might need to enable the HSE Bypass mode.Check the bit clock you see on the USART output by outputting a continuous stream of 0x55 characters.Check the internal clocks of the F3 by outputting via it's MCO PA8 pin.2015-06-24 1:28 AM
Dear community,
Thank you very much for responding to my question.
I forgot to select “PLL && HSE� in the excel- worksheet. The new start- up.c file configures the clock @ 72 MHz which I double-checked at the MCO pin using an oscilloscope.
(http://webcache.googleusercontent.com/search?q=cache:iaiPKKT9sg8J:https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/MCO1%2520output%2520doesn't%2520output%2520anything+&cd=3&hl=de&ct=clnk&gl=de)
Unfortunately the prescaler option of the RCC_MCOConfig command in combination with RCC_MCOSource_PLLCLK has no effect on the output frequency (therefore an oscilloscope with a high sample- frequency is required).
Regarding CLIVE1’s recommendations:
A: Check the bit clock you see on the USART output by outputting a continuous stream of 0x55 characters. -> I did so and found that the baud- rate is twice as high as defined.A: Check the internal clocks of the F3 by outputting via it's MCO PA8 pin.
-> I did so and found that the clock speed is 36*2 Mhz , such as defined
However my USART – issue is still present: The USART speed is twice as high as defined in USART_InitStructure.USART_BaudRate
I will check whether the ''HSE bypass mode'' makes some sense to solve this problem...
2015-06-24 2:47 AM
Dear community,
I did a few experiments by changing the startup.c configuration regarding the APB1 & APP2 prescaler values.
I summarized my result in the following table:
APB1 APB2 Multiplier X (real baudrate = x* baudrate defined)
2 1 0.5
2 4 2
2 2 1
4 8 2
4 2 0.5
4 4 1
Looks like that both APB1 and APB2 must have the same prescaler to get the defined baudrate. I read the reference and also the datasheet but I didn’t found neither an explanation for the obtained result. I would be very happy if someone would explain those findings.
2015-06-24 9:12 AM
Sounds like whatever firmware/library you are using is not correctly associating the USART and APB.
2015-06-26 5:22 AM
To make sure no strange files of different library’s (e.g. older versions from keil and newer version from SPL) are mixed together I made a new project containing only such header files which come together with the standard peripheral library (latest version). No effect. Then I checked the EXCEL clock configuration tool and found that it produced in the wizard mode at least for f30x and f37x controller’s wrong entries for the rcc Registers (see the table in my first post PLLMUL must be 9 and PREDIV must be 1 to reach 72 MHz). In the expert mode it seems to produce more consistent parametrization however I in the case of the f302 it is still as shown in the table of my previous post. Probably it is necessary to check each register entry using reference manual.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.