2014-03-26 1:06 AM
Hi,
Fundamental question here, so please pardon my ignorance. In my interrupt routine I need to modify the EXTI->PR register, however when I set it using the following, EXTI->PR = 0x00000400 After printing out the value, I see it has been changed to 0x00000200 or it may be cleared giving 0x00000000. The interrrupt routine is only entered once as the print statment is only displayed once. Is this the proper syntax to write to EXTI_>PR EXTI-PR? Is this register even read/writeable? Many Thanks Bob2014-03-26 5:59 AM
sorted...writing a 0 to a bit doesn't do anything !!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.