2023-03-19 10:22 PM
Hello, Now I'm using Modbus RTU and UART. Modbus RTU communication is being performed through UART. Modbus RTU setting is data 8 bytes, but communication is possible only when uart wordlength is set to 9 in STMcubeIDE. Why is wordlength 9 when data is 8?
2023-03-19 11:45 PM
Parity bit.
According to the Modbus RTU spec, 2.5.1, support for even parity is required. Other modes (no parity, odd parity) are optional.
2023-03-20 12:37 AM
... and in the STM32 UART, confusingly different from other manufacturers' UARTS, the parity bit is counted up to the total word length.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.