2022-11-04 11:43 AM
2022-11-04 11:55 AM
Bad or poorly constructed code? Optimization tends to highlight latent issues.
Stack size? Alignment?
Clocks, Flash wait-states?
Perhaps have the Hard Fault Handler output some actionable data, the MCU provides a lot of detail, inspect it.
2022-11-04 12:19 PM
Check your variables used global and modified in IRQ is marked _IO or volatile.
2022-11-04 2:39 PM
It might be this
-O2 or above replaces loops and such with library functions, and if you have not got these included then it will crash.
Otherwise, single stepping through the code, and using the stack trace, is the way.
2022-11-07 9:00 AM
how can you capture this, the break point in the HardFault_Handler never hits and the compiler says No source available for "HardFault_Handler() at 0x800dd34"
also seem it occurs before I enter main. A breakpoint in main is never hit.
I guess because I'm debuging the release version?
I even added a trace on one of the GPIO pins to catch it on my scope. I put one at the beginning of the app and one in the main loop. Neither show up. Like the app crashes before it starts.
I am able to step thru the assembly but what would be a way to see the (UFSR) - register.
using the SFR I can see the UFSR register but it's null
Register: CFSR_UFSR_BFSR_MMFSR
Address: 0xe000ed28
Value: null
Size: 32
Reset value: 0x0
Reset mask: 0xFFFFFFFF
Access permission: RW
Read action:
2022-11-08 6:17 AM
Ok here we go found the culprit. Sadly this is not my code ( new guy on the job ) but I know putting in this return prevents the fault
int Read_Flash32(uint32_t address) //Reads 32 bits of data
{ return 0;
// uint32_t temp1;
uint32_t temp;
// temp1 = (uint32_t *)address;
// temp = &temp1;
uint32_t *data;
temp = 0;
data = 0;
*data = *(__IO uint32_t *)address;
temp = *data;
.
.
.
}
So I really need to see my SCB registers for fault reason & location but in release mode I can not. Of course debug code has no fault. How can I do this?
interestingly if I put a trace in my code for some poormans debug I do see it but not if I put it in the Read_Flash32. It would seem the fault is generated by ASM and not by the running code. Putting the return in there seem to negate the fault maybe becase the ASM was not built.
ASM with return
080063a8 <Read_Flash32>:
80063a8: 2000 movs r0, #0
80063aa: 4770 bx lr
ASM with code that cause fault
080063a8 <Read_Flash32>:
80063a8: 2300 movs r3, #0
80063aa: 6802 ldr r2, [r0, #0]
80063ac: 601b str r3, [r3, #0]
80063ae: deff udf #255 ; 0xff
2022-11-08 7:39 AM
huh..
When the compiler analyzed the code, it saw that the pointer had been set to 0. Even though 0 is a reasonable value for our code, it is unlikely to be correct because reading location 0 is not that common.
So putting in the code to halt my program isn’t a bad choice, but the compiler should have generated a message, warning that I was dereferencing a null pointer.
so I can NOT set to 0 or use -fno-delete-null-pointer-checks
?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.