2023-12-15 3:24 AM - last edited on 2023-12-17 12:31 PM by STTwo-32
Hi,
I am facing a problem to connect the B-L4S5I-IOT01A STM32 board to Wifi. I downloaded X-Cube-AWS.
And STM32L4 Discovery Kit IoT Node (B-L475E-IOT01A) ISM43362-M3G-L44-SPI-C3.5.2.7.STM SPI Firmware but still fails to connect.
Please if anyone can provide the steps to connect the wifi module to the mentioned board.
Greetings
Mrinalini
2023-12-17 12:12 PM
Hello @mrinalinibarik,
You can have a look at the WiFi examples of communication between the STM32L4S5 and ISM433 WiFI chips with SPI by looking at STM32Cube L4 FW package in /Projects/B-L4S5I-IOT01/applications/WiFi (Common/Src/Wifi.c and es_wifi.c)
Hope this helped you!
Imen
2024-01-26 5:59 AM
Hello
What WiFi access point are you using ?
Are you using an iPhone or iPad as access point ? If yes, recent versions of iOS use WPA3 for WiFi security and B-L4S5I-IOT01A WiFi module doesn't support it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.