2018-08-20 1:04 PM
Why is the value for stm32f7xx_ll_sdmmc.h's SDMMC_CMDTIMEOUT (5 seconds!) so insanely huge as compared to the Reference Manual SDMMC_STA.CTIMEOUT description and the MMC Ncr timing?
2018-08-20 1:35 PM
You think that's a long time...
#define SDMMC_DATATIMEOUT ((uint32_t)0xFFFFFFFFU)
#define SDMMC_CMDTIMEOUT ((uint32_t)5000U) /* Command send and response timeout */
#define SDMMC_MAXERASETIMEOUT ((uint32_t)63000U) /* Max erase Timeout 63 s */
2018-08-21 5:52 AM
Yeah, I've seen those too. It'd be helpful if there was some commentary explaining such ludicrous values, especially in the case of SDMMC_CMDTIMEOUT, which should rightfully have a value no larger than (64 + 48 + some_small_number) * (SDMMC_CK period).
Hello, ST? 5 seconds checking for bits that should (must!) be set in << 1 mSec?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.