cancel
Showing results for 
Search instead for 
Did you mean: 

Why ST firmware SAI skip 88200Hz (176400 too) as audio samplerate?

MM..1
Chief III

I work with x-cube-usb UAC and see , that define not exist WHY?

/** @defgroup SAI_Audio_Frequency SAI Audio Frequency
  * @{
  */
#define SAI_AUDIO_FREQUENCY_192K          192000U
#define SAI_AUDIO_FREQUENCY_96K           96000U
#define SAI_AUDIO_FREQUENCY_48K           48000U
#define SAI_AUDIO_FREQUENCY_44K           44100U
#define SAI_AUDIO_FREQUENCY_32K           32000U
#define SAI_AUDIO_FREQUENCY_22K           22050U
#define SAI_AUDIO_FREQUENCY_16K           16000U
#define SAI_AUDIO_FREQUENCY_11K           11025U
#define SAI_AUDIO_FREQUENCY_8K            8000U
#define SAI_AUDIO_FREQUENCY_MCKDIV        0U

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Not sure why it is necessary to look for complexity or reason. I'd hazard that your frequencies are atypical, at least in the MPEG CD/DVD or Telco audio standards I've used in the past.

If it is just taking a numeric value for frequency should it need a define at all? Lot of dsylexic devs who can't transcribe numbers in my experience. The constraining factors here typically are the source clocks, PLLs or divider chains. If the RM says you can free-from these numbers, do so.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.