cancel
Showing results for 
Search instead for 
Did you mean: 

Why should in 'G4 PB8/BOOT0 be set to non-Analog?

waclawek.jan
Super User

In 'G4 Datasheets and RM, the following remark can be read:

It is recommended to set PB8 to a different mode than the analog one to limit the
consumption that would occur if the pin is left unconnected.

This must be important, as it's at both in DS and RM, and in RM it's repeated twice (with slightly different wording).

But why?

Isn't Analog the low-power option?

PB8 doesn't even have an Analog functionality.

JW

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Foued_KH
ST Employee

Hello @waclawek.jan , 

I will check this internally.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks, Foued.

Jan

Foued_KH
ST Employee

Hello @waclawek.jan ,

The PB8 pin has no analog switch and therefore cannot be set into analog mode.

 There is need to change PB8 pin into mode which is safe regarding to consumption if it is left unconnected.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

waclawek.jan
Super User

Hi @Foued_KH ,

Sorry, but I don't quite get it.

Is PB8 the only pin which does not have analog switch?

And, would PB8 be set e.g. to Input, how would it be safer regarding to consumption, if left unconnected?

Thanks,

Jan

If voltage on PB8-BOOT0 pin is in the middle of the VDD supply – even if PB8 is configured in analog mode - then there is higher consumption.
PB8 looks like configured in input mode instead of analog mode. This consumption can be caused by PB8 or by BOOT0 pin.
What does happen if BOOT0 signal is floating?
>>The consequence is that if the device is under reset and PB8 pin is floating then there is higher consumption.

Workaround is to configure PB8 in output mode or enable pull-up/down on it.

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Foued,

I clicked on "Accept as solution" by mistake... that last post made me even more confused.

> Workaround is to configure PB8 in output mode or enable pull-up/down on it.

The multiple remarks in DS and RM don't state this.

>>The consequence is that if the device is under reset and PB8 pin is floating then there is higher consumption.
> Workaround is to configure PB8 in output mode or enable pull-up/down on it.

Under reset, how can I configure PB8 in output mode etc.?

Can you please quantify the "higher consumption"?

Thanks,

Jan

@Foued_KH 

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.