2016-02-05 2:16 AM
I am working with the ST-Link Discovery development board and I'm trying to get the SPI-bus working properly. I have configured SPI1 as my master and SPI2 as my slave and I connected wires in between them. I have verfied with a logic analyzer that my master is working great. However, my slave seems hopeless, no matter what I do I don't get any interrupts. Can someone please help me?
void initializeSpi2controlPins(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/***************************************************
***************** SPI MISO ***********************
***************************************************/
GPIO_InitStructure.Pin = GPIO_PIN_2;
GPIO_InitStructure.Mode = GPIO_MODE_AF_PP;
GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
/***************************************************
***************** SPI MOSI ***********************
***************************************************/
GPIO_InitStructure.Pin = GPIO_PIN_3;
GPIO_InitStructure.Mode = GPIO_MODE_AF_OD;
GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
/***************************************************
***************** SPI CLK ************************
***************************************************/
GPIO_InitStructure.Pin = GPIO_PIN_10;
GPIO_InitStructure.Mode = GPIO_MODE_AF_OD;
GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
/***************************************************
***************** SPI NSS ************************
***************************************************/
GPIO_InitStructure.Pin = GPIO_PIN_9;
GPIO_InitStructure.Mode = GPIO_MODE_AF_OD;
GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Alternate = GPIO_AF5_SPI2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStructure);
}
void enableSpi2module(void)
{
SPI_HandleTypeDef hspi;
hspi.Instance = SPI2;
hspi.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi.Init.Direction = SPI_DIRECTION_2LINES;
hspi.Init.Mode = SPI_MODE_SLAVE;
hspi.Init.DataSize = SPI_DATASIZE_16BIT;
hspi.Init.NSS = SPI_NSS_HARD_INPUT;
hspi.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi.Init.TIMode = SPI_TIMODE_DISABLE;
RCC->AHB3ENR |= RCC_APB1ENR_SPI2EN; // Enable clock for SPI 2
if (HAL_SPI_Init(&hspi) != HAL_OK)
{
INV_UART4_TransmitNullTerminatedString((uint8_t*)''\r\nSPI2. Initialization Error'');
INV_UART4_WaitForTransmitToFinish();
}
__HAL_SPI_ENABLE(&hspi);
__HAL_SPI_ENABLE_IT(&hspi, (SPI_IT_TXE | SPI_IT_RXNE | SPI_IT_ERR));
HAL_NVIC_EnableIRQ(SPI2_IRQn); // Enable SPI bus interrupts
SPI2->CR1 |= SPI_CR1_SPE;
SPI2->CR2 |= SPI_CR2_RXNEIE;
SPI2->CR2 |= SPI_CR2_ERRIE;
SPI2->CR2 |= SPI_CR2_TXEIE;
}
void SPI2_IRQHandler(void)
{
INV_UART4_TransmitNullTerminatedString((uint8_t*)''\r\nSPI2_IRQHandler.'');
INV_UART4_WaitForTransmitToFinish();
}
2016-02-05 3:09 AM
Maybe I should add that I do make sure to enable the clocks to the pins, I do that in a different file:
void RCC_Configuration(void)
{
RCC->APB1ENR |= RCC_APB1ENR_UART4EN; // Enable clock for UART 4
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; // Enable clock for GPIO port A
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN; // Enable clock for GPIO port B
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOCEN; // Enable clock for GPIO port C
RCC->AHB1ENR |= RCC_AHB1ENR_GPIODEN; // Enable clock for GPIO port D
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOEEN; // Enable clock for GPIO port E
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOFEN; // Enable clock for GPIO port F
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOGEN; // Enable clock for GPIO port G
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOHEN; // Enable clock for GPIO port H
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOIEN; // Enable clock for GPIO port I
}
2016-02-05 3:38 AM
I tried to dump all SPI2-registers in the end of the enableSpi2module function and all I read are zeros(!):
SPI2->CR1: 0x0SPI2->CR2: 0x0SPI2->CRCPR: 0x0SPI2->DR: 0x0SPI2->I2SCFGR: 0x0SPI2->I2SPR: 0x0SPI2->RXCRCR: 0x0SPI2->SR: 0x0SPI2->TXCRCR: 0x0Anybody got a theory on what's going on here?2016-02-05 3:59 AM
I found the problem. I was turning on the wrong clock:
RCC->AHB3ENR |= RCC_APB1ENR_SPI2EN; // Enable clock for SPI 2
should have been
RCC->APB1ENR |= RCC_APB1ENR_SPI2EN; // Enable clock for SPI 2
2016-02-05 8:41 AM
Thats why you should keep an eye on the numbers in the define and the register.
Your symptoms are typical for ''clock not enabled''. So for the future, it may help you to know that if all (or many) registers read as zero, you might have forgotten to enable the clock.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.