2019-07-18 12:47 AM
I use MCU STM32L073, set VDDA=VREF+=3.29V, VSSA=VREF-=GND=0V.
I read Vrefint_cal for (0x1FF80078), get the value of Vrefint_cal = 0x680
get Vrefint_data from ADC_CHANNEL_17, get this value is Vrefint_data =0xbb7
the code is here:
////////////////////////////////////////////////////////////
HAL_ADCEx_EnableVREFINT();
sConfig.Channel = ADC_CHANNEL_17;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
//open adc
if (HAL_ADC_Start(&hadc) != HAL_OK)
{
Error_Handler();
}
HAL_ADC_PollForConversion(&hadc, 100);
if ((HAL_ADC_GetState(&hadc) & HAL_ADC_STATE_REG_EOC) == HAL_ADC_STATE_REG_EOC)
{
/* Get the converted value */
Vrefint_data = HAL_ADC_GetValue(&hadc);
}
Vrefint_cal=*(__IO uint32_t*)(0x1FF80078);
Vdda=3.3*(Vrefint_cal)/Vrefint_data;
printf("Vrefint_cal=%#x,Vrefint_data=%#x Vdda=%#f\r\n",Vrefint_cal,Vrefint_data,Vdda);
//////////////////////////////////////////////////////////
use Vdda=3.3*(Vrefint_cal)/Vrefint_data; I cout vdda = 1.831010, not 3.9V , why???
2019-07-18 2:10 AM
Wow, VDDA = 3.9 V is very near the absolute maximum of 4.0 V. As VDDA- VDDx is 0.3 Volt Maximum, this means with VDDA=3.3 Volt you will get a lot of imjected current and nonsense ADC values. With some overshoot on VDDA, the snalig section may also be damaged already.
2019-07-21 7:27 PM
sorry, I tested the wrong place to get the VDDA value before . i already changed it , please help me to check the question again ,thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.