2023-02-19 9:20 PM
I am using a Nx_Webserver application example from STM32H735G-DK modified for STM32H743i-Eval. I have moved the Rx, Tx, NetXPool references to RAM_D2 and I find that I get an error when the linker runs if the RxDecripSection and TxDecripSection name matches that which is in main. If the names are different it links fine and the map shows the sections mentioned in 0x240xxxxx. Not what I want.
the likker script looks like this:
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200; /* required amount of heap */
_Min_Stack_Size = 0x400; /* required amount of stack */
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
/* Define output sections */
SECTIONS
{
/* The startup code goes first into FLASH */
.isr_vector :
{
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} >FLASH
/* The program code and other data goes into FLASH */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
_etext = .; /* define a global symbols at end of code */
} >FLASH
/* Constant data goes into FLASH */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >FLASH
.ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >FLASH
.ARM : {
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} >FLASH
.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} >FLASH
.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} >FLASH
.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} >FLASH
/* used by the startup to initialize data */
_sidata = LOADADDR(.data);
/* Initialized data sections goes into RAM, load LMA copy after code */
.data :
{
. = ALIGN(4);
_sdata = .; /* create a global symbol at data start */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
*(.RamFunc) /* .RamFunc sections */
*(.RamFunc*) /* .RamFunc* sections */
. = ALIGN(4);
_edata = .; /* define a global symbol at data end */
} >RAM_D1 AT> FLASH
/* Uninitialized data section */
. = ALIGN(4);
.bss :
{
/* This is used by the startup in order to initialize the .bss section */
_sbss = .; /* define a global symbol at bss start */
__bss_start__ = _sbss;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
_ebss = .; /* define a global symbol at bss end */
__bss_end__ = _ebss;
} >RAM_D1
/* threadX heap section*/
._threadx_heap :
{
. = ALIGN(8);
__RAM_segment_used_end__ = .;
. = . + 64K;
. = ALIGN(8);
} >RAM_D1 AT> RAM_D1
/* User_heap_stack section, used to check that there is enough RAM left */
._user_heap_stack :
{
. = ALIGN(8);
PROVIDE ( end = . );
PROVIDE ( _end = . );
. = . + _Min_Heap_Size;
. = . + _Min_Stack_Size;
. = ALIGN(8);
} >RAM_D1
/* Networking resources */
.tcp_sec (NOLOAD):
{
. = ABSOLUTE(0x30000000);
*(.RxDecripSection)
. = ABSOLUTE(0x30000060);
*(.TxDecripSection)
} >RAM_D2
.nx_data (NOLOAD):
{
. = ABSOLUTE(0x30000100);
*(.NxServerPoolSection)
. = ABSOLUTE(0x30004100);
*(.NetXPoolSection)
} >RAM_D2
/* Remove information from the standard libraries */
/DISCARD/ :
{
libc.a ( * )
libm.a ( * )
libgcc.a ( * )
}
.ARM.attributes 0 : { *(.ARM.attributes) }
}And the relevant section in main private variables looks like this:
ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection"))); /* Ethernet Rx DMA Descriptors */
ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection"))); /* Ethernet Tx DMA Descriptors */the sections defined for .nx_data are no problem. And before you ask, I do have the global define USE_D2_RAM set. So what did I miss?
Solved! Go to Solution.
2023-02-20 7:20 AM
Correcting myself. What I originally missed is the fact that in all the application examples for web servers, the discriptors are set to 4 not 0x60 which is the length required to hold 4 of them. Going back to a fresh project creation for STM32H743i-eval with default values selected for the peripherals, CubeMX sets the ETH parameters of TX and Rx Descriprtor lengths to 4 but the First Tx Descriptor Address is 0x30000200 not 0x30000060 like all the examples. I also notice that the build will use D2 ram but nothing is in the linker script to make that happen so the compiler is mapping them to D1 ram. So when is CubeMX going to start configuring the linker scripts so what you see in CubeMX is what you get? Seems like all time I wasted figuring this out could have been avoided. I also think that in ETH parameter settings the name "Tx Descriptor Length" is a little misleading. I would have preferred "Tx Descriptors" meaning "how many".
KnarfB - Thanks Again for the prompt!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.