2017-02-01 1:14 PM
I'm trying to implement a SPI slave on STMF410 using NSS_HARD_INPUT
Slave should receive data of unknown length via DMA
Slave transmissions are of known length so master knows to keep the SlaveSelect line active for the correct time.
I'm am expecting that when SS line is released, DMA should complete and execute the DMA complete IRQ
But ifI initial the DMA with the PFCTRL bit set, I no longer get the DMA IRQ to execute.
The Tx DMA never becomes READY and is always BUSY
Has anybody else tried SPI Slave with PFCTRL
2017-02-01 2:07 PM
I'm trying to implement a SPI slave on STMF410
Do you mean STM32F410?
I'm am expecting that when SS line is released, DMA should complete and execute the DMA complete IRQ
Why are you expecting that, have you seen such behaviour described in the documentation (RM0401, namely)?
But ifI initial the DMA with the PFCTRL bit set, I no longer get the DMA IRQ to execute.
That is expected. In STM32F410 there is no peripheral capable of being the Flow Controller, see RM0401 rev.2, ch. 8.3.15 Flow controller (it's written there in a cumbersome way resulting probably from automatic datasheet generation, as no peripherals listed after the 'This feature is only supported for peripherals which are able to signal the end of the transfer, that is:' sentence).
There is a
https://community.st.com/community/stm32-community/stm32-forum/blog/2016/12/30/2017-stm32-wish-list
active currently, where you can propose STM32 hardware enhancements; don't expect they materialize anytime soon if at all.JW
2017-02-01 3:16 PM
Yes STM32F410
The behavior was IMPLIED in the datasheet, but I now see where the list of (STM32F410) peripherals that support this feature is <null>
Thanks for your VERY QUICK response.
2017-02-14 1:50 AM
Referring to
, only SD/MMC and JPEG peripherals support Flow Control mode.-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.