2018-11-08 4:35 AM
DMA1_Stream0->FCR = 0
DMA configured to work in double buffer direct mode.
And I get FEIF0 error interrupt flag?
2018-11-08 4:51 AM
Same problem for me also ( but I don't use a double buffer).
The FEIFx bit is being set when the DMA stream is enabled(EN = 1) in the DMA_SxCR.
Interestingly, it seems to happen only with Memory to Peripheral transfer.
2018-11-08 10:28 PM
This is the expected behaviour in the 'F2/'F4/'F7 DMA, see the note in 4.3 Software sequence to enable DMA in AN4031.
In Direct mode, simply ignore this flag, i.e. don't enable DMA_SxFCR.FEIE.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.