2022-12-09 6:25 AM
So I am setting up the DMA for USART1 tx on a STM32F4 on each transfer, and busy wait for it to be done (no interrupt) by polling TC.
DMA2_Stream7->NDTR = len;
DMA2_Stream7->PAR = (uint32_t)&(USART1->DR);
DMA2_Stream7->M0AR = (uint32_t)str;
DMA2_Stream7->FCR |= DMA_SxFCR_DMDIS;
DMA2_Stream7->CR = (0x4 << DMA_SxCR_CHSEL_Pos) | DMA_SxCR_MINC | DMA_SxCR_DIR_0 | DMA_SxCR_PL_1 | DMA_SxCR_PL_0 | DMA_SxCR_MSIZE_1;
USART1->CR3 |= USART_CR3_DMAT;
USART1->SR &= ~USART_SR_TC;
DMA2_Stream7->CR |= DMA_SxCR_EN;First I ran without FIFO, (Direct mode), but that gave also FEIF and lost tx data. After enabling the FIFO, all data seems to be sent, but I still get the FEIF after each tx block.
I tried to reduce the baud rate down to 115200, but I still get the FEIF error...
Even if I only send 4 bytes, I get the FEIF, so I figure I must have configured something wrong.
I get TCIF on each send, and I think everything is actually sent fine.
Any help appreciated!
Solved! Go to Solution.
2022-12-09 6:30 AM
Enable the DMA stream (set DMA_CR.EN) *before* you enable the DMA on peripheral (USART1_CR3.DMAT).
Read AN4031 4.3 Software sequence to enable DMA
JW
2022-12-09 6:30 AM
Enable the DMA stream (set DMA_CR.EN) *before* you enable the DMA on peripheral (USART1_CR3.DMAT).
Read AN4031 4.3 Software sequence to enable DMA
JW
2022-12-09 6:47 AM
Wow, thanks a lot!
I clearly must be blind, or have some kind of deficiency ; I have read AN4031 several times without seeing that part. :grinning_face:
Now it works just as it is supposed to.
Cheers,
Micael
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.