2011-03-14 11:53 AM
While problem
2011-05-17 5:27 AM
Is the variable delay_main is of volatile type ?
__IO uint32_t delay_main;
2011-05-17 5:27 AM
2011-05-17 5:27 AM
do I miss something here ?
Define it as volatile so the compiler doesn't optimize it to an infinite loop. ie it changes outside the context of the current routine.2011-05-17 5:27 AM
Thank you
is not unsigned int a volatile ? since I define it under the include headers directly . where can I fine the type of definisions for keil for the new lib 3.4 ?2011-05-17 5:27 AM
is not unsigned int a volatile ? since I define it under the include headers directly .
No, being external or publically defined is not the same as being volatile, which infers that it might change between different reads. Like a hardware register, or interrupt incremented counter. volatile unsigned int delay_main;2011-05-17 5:27 AM
2011-05-17 5:27 AM
sorry I am back with new question , exuce me I am new to cortex m3 and STM
my system coreclock is 72Mhz , I want the system tike inturrept every 5ms so how can I calculate this what is the formula? what is the relation between tick and ms? if(SysTick_Config(SystemCoreClock / x) ) // 5ms interrupts x=? the formula please . Thank you2011-05-17 5:27 AM
what is the relation between tick and ms? what is the diffrent between static and volatile in this case ?
1/1000 th of a second is 1ms, x = 1000 5ms period is 1000/5 thus x = 200, ie 5/1000 th of a second or 1/200 th of a second. Measured in 72 MHz cycles, where 72000000 cycles per second 72000 cycles per millisecond, and 360000 cycles per 5 milliseconds. A static is invisible outside the current object file. You should use volatile if the value changes independent of program flow. ie in an interrupt. If you call a subroutine it is assumed variables will change. You could also turn off optimization, and then the compiler wouldn't hold variables in registers, or reduce loops.
2011-05-17 5:27 AM
Thank you alot Clive
if(SysTick_Config(SystemCoreClock / 360000) ) // 5ms interrupts
returns an error that cant load it ; any solution for 5ms interrupt? I am using the new library 3.4. RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.