2020-10-28 12:43 AM
The CAN transceiver IC, i am using : TJA1057GT/3 , and I am seeing the some data waveform on oscilloscope but decoding is not happening. the baud rate varies for the CAN FD is from ~300kbps to 1Mbps(large fluctuation).
Clock Divider : Divide kernel clock by 1
Frame Format : FD mode without BitRare Switshing
Mode : Normal Mode
Auto Retransmission : Enable
Transmit Pause : Enable
Protocol Exception : Disable
Nominal Prescaler : 1
Nominal Sync Jump Width : 16
Nominal Time Seg1 : 63
Nominal Time Seg2 : 16
Data Prescaler : 2
Data Sync jump width : 4
Data time Seg 1 : 5
Data time Seg2 : 4
Std Filters Nbr : 1
Ext Filter Nbr : 0
Tx Fifo Queue Mode : FIFO mode
Above is the configuration for Cube IDE, can some one help me what could be the solution to resolve the issue
2020-10-28 12:49 AM
this is the configuration i am using
2020-10-28 1:20 AM
2020-10-31 2:02 PM
Hi,
Try to measure the resistance between Can wires. It should be 120 Om.
If not Check the can analyzer maybe on t you will find switch "terminator"
If not connect the resistor ( 60 or 120 Om) from any side.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.