2018-01-30 11:12 PM
I found that I can adjust UART RX pin active level inversion in CubeMX with STM32F303
but there is no such selection with STM32F405I wonder which chip support that function
2018-01-31 3:15 PM
'F0, 'F3, 'F7, 'H7, 'L0, 'L4
JW
2018-01-31 4:43 PM
>>I wonder which chip support that function
If in doubt consider reviewing the Reference Manual, usually has such details.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.