2015-04-29 5:24 AM
I bought a discovery board with STM32F4 family processor (comes with a TFT LCD). I have my IDE working and downloaded CubeMX and generated some init code - no problem.
Now, I don't know how to do anything! How do I toggle a pin? How do I use the peripherals? Where is all that sort of data written?I went through all the files in the discovery board page and nothing really helpful in there. The only thing I have managed to understand is that CubeF4 is contains libraries and drivers that I can use to simplify development. But is there any text on these? A datasheet of some sorts that also explains a bit about the architecture? #discovery #stm23f4 #getting-started2015-04-29 5:33 AM
Data for chip, and design support information.
http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1577/LN1806/PF255419
I'd recommend the Standard Peripheral Library over Cubehttp://www.st.com/web/en/catalog/tools/PF257901
And the firmware examples for the STM32F429I-DISCOhttp://www.st.com/web/en/catalog/tools/PF259429
Ignore the Cube messaging, go to the Red Download buttons at the bottom of the pages. Should be a Windows Help file in the root directory of one of the packages.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.