2020-04-25 5:52 AM
Hello,
i read the UM2577 pdf, the user manual for the Discovery kit with STM32G474RE MCU (B-G474E-DPOW1 board). On page 29, chapter 13.3, an audio class-D amplifier example with separate application note is mentioned. Where can i find this app note and/or the example?
Kind regards,
Greg
2020-04-27 3:15 AM
Perhaps it is also confidential, like the source code of AN5142?
https://community.st.com/s/question/0D50X0000BqAlXeSQK/an5142
Personally, it would be interesting to get further information about H-bridge PWM programming with STM32 HRTIM for Class-D amp application.
But i understand that ST also wants to sell their Class-D Amplifier IC... ;)
Are there any other app notes, manuals etc. covering PWM H-bridge (class-D) programming with MCUs, preferably from ST, anyone can recommend? Thanks in advance.
2020-05-04 4:17 AM
Hi @GregKN ,
I think that AN5142 (Class-D audio amplifier implementation on STM32 32-bit Arm® Cortex® MCUs). Right?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.