2015-10-29 12:59 AM
Hi all,
Recently I am working on a demon code using STM32F103.In this demon code,it defines the PE2, PE3 as the I2C interface, as below:/* Configure I2C pins: PE2->SCL and PE3->SDA */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 ;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode =GPIO_Mode_Out_PP ;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP ;
GPIO_Init(GPIOE, &GPIO_InitStructure);
/* ---------------------------------------------------- */However, I checked through the reference manual and datasheet, it claims F103 has 2 I2C interface, but very few information on the 2nd I2C, such as AF of which pin are defined as I2C.In datasheet Pin information chapter, it syas:PE2 : TRACECK/ FSMC_A23
PE3 : TRACED0/FSMC_A19
So, Trace function pins, CK and Data0, can be configured as I2C2? I checked the code of later parts, I found code as :/* ---------------------------------------------- */static void I2C_SendByte(uint8_t SendByte)
{
uint8_t i=8;
while(i--)
{
//SCL_L;
//I2C_delay();
if(SendByte&0x80)
SDA_H;else SDA_L;
SendByte<<=1;
I2C_delay();
SCL_H;
I2C_delay();
SCL_L;
I2C_delay();
}
}
&sharpdefine SCL_H GPIOE->BSRR = GPIO_Pin_2
&sharpdefine SCL_L GPIOE->BRR = GPIO_Pin_2
&sharpdefine SDA_H GPIOE->BSRR = GPIO_Pin_3
&sharpdefine SDA_L GPIOE->BRR = GPIO_Pin_3
/* -------------------------------------------------------------- */So, it seems like the code actually use GPIO of PE2, PE3 to mimic the operation of I2C, it didn't use any I2C related register. Right? #i2c22015-10-29 1:18 PM
2015-10-30 1:19 AM
I noticed PE2->SCL and PE3->SDA pins are configured as push-pull.
GPIO_InitStructure.GPIO_Mode =GPIO_Mode_Out_PP
Normally, they would be Open Drain.
In defence of bit banging I2C - it's often the simplest and most trouble free way to do it especially if the manufacturer's implementation of I2C in the silicon is poor.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.