2016-08-16 3:56 PM
I should use the USB FS on CN5 of STM32F4-Discovery in dual Virtual Com Port (if possible in three VCP).
I made a project started from cubemx with USB_CDC_VCP with USBD_MAX_NUM_INTERFACES = 3 and USBD_MAX_NUM_CONFIGURATION=3 .It work well but in the pc instal one COM only.I tryed to modify the usb descriptor manually but it not work fine. I have Always one COM only.Where i can find un example based on cubemx library whith multiple CDC VCP?Very Thank.2016-08-17 2:35 AM
Hi lor3n7o,
USB composite isn't supported yet by CubeMX.I report your request internally for farther review. We will keep you informed if we have more details on this regard.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2016-08-17 2:58 AM
Very thanks for faster support.
2016-08-19 1:01 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.