2025-07-17 6:14 AM - last edited on 2025-07-17 6:42 AM by Andrew Neil
Hello,
MCU: STM32L071
During a transition from RDP level 1 to RDP level 0 the MCU stays stalled.
Only a power supply off then on permits to have it running.
Do you have any suggestion?
Best regards
Mich
2025-07-17 6:41 AM
Hello @mich35
As described in the reference manual RM0377:
Note: If the read protection is set while the debugger has been active (through SWD) after last POR (power-on reset), apply a POR (power-on reset) or wakeup from Standby mode instead of a system reset (the option bytes loading is not sufficient).
Try reload the option bytes after programming, for that you can refer to the "3.8.3 Reloading Option bytes by software"section in the reference manual RM0377.
2025-07-17 8:11 AM
Hello Imen,
I was not with the debugger.
I try to put the system in Standby mode but it does not work, the MCU is stalled. (it works fine from level 0 to level 1)
I follow "STM32 Security tips - 3 RDP without POR" video (level 0 to level 1) but there is nothing for level 1 to level 0.
Best regards
Michel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.