2016-03-22 2:12 AM
I have recently reversed-engineer some HAL source code and I see that sometimes a temporary variable is used to manipulate a register, for example
uint32_t tmp = 0;
tmp = hdma->Instance->CR;
tmp |= hdma->Init.MemBurst | hdma->Init.PeriphBurst;
hdma->Instance->CR = tmp;
At other times, the register is changed directly, for exaple:
#define __HAL_SPI_ENABLE(__HANDLE__) ((__HANDLE__)->Instance->CR1 |= SPI_CR1_SPE)
What is the rule here?
2016-03-22 2:42 AM
No such rule.
Generally, you want to avoid multiple accesses to reduce execution time and code memory consumption. Many if not most RMW you see in examples/''libraries'' are unnecessary, you simply write the value you want to be in the register, the value of reserved bits is given in RM. There are registers where extra accesses have side effects, common sense applies there. Forget about Cube, RM is your friend. JW2016-03-22 2:51 AM
They expect the compiler to tighten things up.
With a tmp variable there is the potential to gain more efficiency as the compiler can fold multiple operations, some thing it can't do with volatile peripheral registers directly.2016-03-22 5:00 AM
Hi arnold_w,
We apply the direct access in the macro because we have to do just a single access update to the register (only one bit-field). I f we have multiple access, we ought to use temporary variable to gain R/W operations. -Hanniba-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.