2023-11-06 6:44 AM
The ref manual (RM0481 page 2585) says: "This circuit has a defined startup time (tSTARTUP specified in the datasheet) during which the behavior of the USB transceiver is not defined.". I searched for USB and tSTARTUP but could not find anything in the datasheet (DS14258 Rev 1). Is it missing or mentioned differently ?
Solved! Go to Solution.
2023-11-07 2:28 AM
Hello @mete ,
The USB tSTARTUP is missing in the datasheet.
I reported this issue internally.
Internal ticket number: 165751 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-06 7:31 AM - edited 2023-11-06 7:40 AM
Hello @mete ,
Thank you for bringing this issue to our attention.
I will check internally and I will get back to you with more details as soon as possible.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-07 2:28 AM
Hello @mete ,
The USB tSTARTUP is missing in the datasheet.
I reported this issue internally.
Internal ticket number: 165751 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-07 6:01 AM
Thanks. I have seen it is written in the datasheet of STM32H503, and it is 1us. Can I assume it is going to be the same for H563 as well ?
2023-11-08 2:14 AM - edited 2023-11-08 2:15 AM
Hello @mete ,
Yes, the STM32H563 has the same USB tSTARTUP "1µs" as STM32H503.
Thank you for your contribution in STCommunity.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-15 4:04 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.