2020-06-19 12:12 PM
Hi,
I am new to STM32 platform. I am using the STM32F439 Nucleo-144 board and STM32CubeIDE. I noticed that in the STM32Cube graphic interface, I can't find anything for SSL/TLS? I did read about Polar SSL but I can't find it anywhere in the interface or in any of the folders. I also can't find it under third party. Even wolfSSL. So my question is, what TLS is used for this? And where can I get it/how can I add it to the STM32Cube project? I'm planning to add TLS to my TCP project.
Thanks.
AJ
Solved! Go to Solution.
2020-06-19 12:20 PM
I think I just found the answer to my question. It looks like it's MBEDTLS. I have never used or heard of it before. Are there any available examples for TCP client and server applications? I checked the STM32F4Cube folder under projects and boards and applications but did not see any MBEDTLS examples.
Thanks again
AJ
2020-06-19 12:20 PM
I think I just found the answer to my question. It looks like it's MBEDTLS. I have never used or heard of it before. Are there any available examples for TCP client and server applications? I checked the STM32F4Cube folder under projects and boards and applications but did not see any MBEDTLS examples.
Thanks again
AJ
2020-06-19 12:26 PM
I am not interested in this at all.
I guess you have to search at mbed.com
JW
2020-06-19 1:46 PM
Hi JW,
Thanks for the info.
Regards,
AJ
2020-06-19 1:54 PM
It looks like wolfSSL also supports STM32F4's. I'm curious, does anyone have some feedback on using wolfSSL vs MBEDTLS? I appreciate any input. My plan to start with simple TCP socket client and server program using LWIP BSD. This is just sort of a quick used case. And then from there, add the TLS. From experience, I've found it easy to migrate my client/server socket code to wolfSSL. Just wondering if it's the same with MBEDTLS. So far, the advantage I see from MBEDTLS is that I just need to enable it on CubeMX. However, I currently have no idea how much changes I would have to do to my socket program.
Thanks.
AJ
2020-06-19 8:34 PM
Hi,
How do I close this thread? I found an MBEDTLS exampls code on one of the project folders in the STM32CubeF4 package.
2020-06-20 12:46 AM
You don't close it but select the correct answer.
And be warned on this:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.