2011-12-03 1:50 AM
I want to create fading Led with pwm, but my code doesn't works. If I simply set bit 1 to pin my led is lights.Please help me.
I'm use stm32f103vet6.int main(void){ GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct; TIM_OCInitTypeDef TIM_OCInitStruct; RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO, ENABLE ); RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM3, ENABLE ); // Set the Vector Table base address at 0x08000000. NVIC_SetVectorTable( NVIC_VectTab_FLASH, 0x0 ); NVIC_PriorityGroupConfig( NVIC_PriorityGroup_4 ); // Configure HCLK clock as SysTick clock source. SysTick_CLKSourceConfig( SysTick_CLKSource_HCLK ); GPIO_StructInit(&GPIO_InitStructure); // Reset init structure // Setup Blue LED on STM32-Discovery Board to use PWM. GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; // Alt Function - Push Pull GPIO_Init( GPIOB, &GPIO_InitStructure ); GPIO_PinRemapConfig( GPIO_FullRemap_TIM3, ENABLE ); // Map TIM3_CH3 to GPIOC.Pin8 // Let PWM frequency equal 100Hz. // Let period equal 1000. Therefore, timer runs from zero to 1000. Gives 0.1Hz resolution. // Solving for prescaler gives 240. TIM_TimeBaseStructInit( &TIM_TimeBaseInitStruct ); TIM_TimeBaseInitStruct.TIM_ClockDivision = TIM_CKD_DIV4; TIM_TimeBaseInitStruct.TIM_Period = 1000 - 1; // 0..999 TIM_TimeBaseInitStruct.TIM_Prescaler = 240 - 1; // Div 240 TIM_TimeBaseInit( TIM3, &TIM_TimeBaseInitStruct ); TIM_OCStructInit( &TIM_OCInitStruct ); TIM_OCInitStruct.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStruct.TIM_OCMode = TIM_OCMode_PWM1; // Initial duty cycle equals 0%. Value can range from zero to 1000. TIM_OCInitStruct.TIM_Pulse = 999; // 0 .. 1000 (0=Always Off, 1000=Always On) TIM_OC3Init( TIM3, &TIM_OCInitStruct ); TIM_UpdateDisableConfig(TIM3,ENABLE); TIM_Cmd( TIM3, ENABLE ); while (1);} #pwm #led #stm32 #stm32f1032011-12-03 1:35 PM
Not GPIOB ! If you want to use PC.8 = TIM3_CH3 (remapped), initialize the GPIOC clock, and GPIOC pin. If you really want in on GPIOB you must not remap it, and it will come out PB.0
pulse width = 999, is pretty much totally ON (a multimeter will read 3.xV). If you want it to pulse 500 might be a better initial value. And probably needs to be much lower to appear DIM. If you want it to phase DIM/BRIGHT you will need to shovel different cyclic PWM values via DMA or at the update interrupt.2011-12-04 12:49 AM
Thanks. I was wrong.I now
get
to control
how
bright
is
the light.Can you please show how to update value of brightness?
2011-12-04 9:39 AM
You can use the library function but I find it just as easy to use:
TIM_SetCompare3(TIM3, 200);
2011-12-04 10:00 AM
Thank you so much
!
You
have helped me
incredibly
.
2011-12-04 10:40 AM
You're welcome. Actually, what I meant to say is this (which will save you about 12 bytes of code space over the previous way), but either method will work.
TIM3->CCR3 = 200;
2011-12-04 1:02 PM
Thanks. A also viewed this on
https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/DispForm.aspx?ID=422&RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Example PWM on STM32-Discovery Blue LED&Source=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/flat.aspx?RootFolder%3D%252Fpublic%252FSTe2ecommunities%252Fmcu%252FLists%252FSTM32VLDiscovery%252FExample%2520PWM%2520on%2520STM32-Discovery%2520Blue%2520LED%26FolderCTID%3D0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51%26currentviews%3D591
But my delay was very little so I don't saw changes, now I'm set it to (80000-200000) and all goes perfect.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.