2019-07-31 3:06 AM
hello everyone,
can someone help me please, I can't understand why I can't receive 7, it's weird...
I sent 7 , i want to receive 7, but I receive 255, 0, 15.. all the values except 7, that's really insane.
2019-07-31 4:32 AM
this code for the F413H:
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hspi->Instance==SPI3)
{
/* USER CODE BEGIN SPI2_MspInit 0 */
/* USER CODE END SPI2_MspInit 0 */
/* Peripheral clock enable */
/*Enable SPI clock*/
__HAL_RCC_SPI3_CLK_ENABLE();
/*Enable GPIO SPI clock*/
__HAL_RCC_GPIOB_CLK_ENABLE();
/**SPI2 GPIO Configuration
PB4 ------> SPI3_MISO
PB5 ------> SPI3_MOSI
PB12 ------> SPI3_SCK
*/
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/*GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI3;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);*/
/* USER CODE BEGIN SPI2_MspInit 1 */
/* USER CODE END SPI2_MspInit 1 */
}
}
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Enable GPIO SPI clock*/
__HAL_RCC_GPIOB_CLK_ENABLE();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_15, GPIO_PIN_RESET); // CS
GPIO_InitStruct.Pin = GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
this code for the f411E:
void HAL_SPI_MspInit(SPI_HandleTypeDef *hspi)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Enable GPIO TX/RX clock */
SPIx_SCK_GPIO_CLK_ENABLE();
SPIx_MISO_GPIO_CLK_ENABLE();
SPIx_MOSI_GPIO_CLK_ENABLE();
/* Enable SPI clock */
SPIx_CLK_ENABLE();
/* SPI SCK GPIO pin configuration */
GPIO_InitStruct.Pin = SPIx_SCK_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = SPIx_SCK_AF;
HAL_GPIO_Init(SPIx_SCK_GPIO_PORT, &GPIO_InitStruct);
GPIO_InitStruct.Pin = SPIx_MISO_PIN;
GPIO_InitStruct.Alternate = SPIx_MISO_AF;
HAL_GPIO_Init(SPIx_MISO_GPIO_PORT, &GPIO_InitStruct);
GPIO_InitStruct.Pin = SPIx_MOSI_PIN;
GPIO_InitStruct.Alternate = SPIx_MOSI_AF;
HAL_GPIO_Init(SPIx_MOSI_GPIO_PORT, &GPIO_InitStruct);
}
static void MX_GPIO_init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
__HAL_RCC_GPIOA_CLK_ENABLE();
//__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_9, GPIO_PIN_RESET);
GPIO_InitStruct.Pin = GPIO_PIN_1;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
what do you think about the configuration?
2019-07-31 5:22 AM
What with SPI configuration? Who master, who slave?
2019-07-31 5:26 AM
I don't see any problem in my eyes, I still suspect this is hardware problem because sending and receiving 1 byte shouldn't be that problematic. Please confirm if data is correctly put into the wire with a oscillator/multimeter/logic analyzer(one easy way is to send 170 instead of 7, in that case miso pin has a frequency=CLK/2 and duty cycle=50%), if no it is sending software problem, but if yes than it is wire/receiver software problem.
2019-07-31 5:30 AM
@oleksandr.karbivsky the F413H is the slave and the F411E is the master!
2019-07-31 5:31 AM
@JChau I'll see that, else I'll use the CAN bus and I'll try with UART too
2019-07-31 5:34 AM
Share SPI configuration for both devices.
2019-07-31 5:35 AM
Yes please, because you have three unknown parts in your situation, sender/wire/receiver, so it is better to isolate the no-problem part 1 by 1.
2019-07-31 7:23 AM
@JChau if it’s the receiver is there any solution?
2019-07-31 7:24 AM
@oleksandr.karbivsky I described it above
2019-07-31 7:57 AM
You confirmed signal bits arrived the receiver correctly? If that's the case the only solution is to check the receiver code, you can also add a breakpoint in stm32f4xx_hal_spi.c line 697 and check the DR register by yourself when receiving in F413H. btw line 697 should reads like this:
/* Check the RXNE flag */
if(__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_RXNE))
{
/* read the received data */
(* (uint8_t *)pData)= *(__IO uint8_t *)&hspi->Instance->DR; //<--THIS LINE
pData += sizeof(uint8_t);
hspi->RxXferCount--;
}if DR register is indeed 0, it means hardware do really receive 0 so you must check again sender/wire. BTW you can also check DR in transmit in line 552 (in this case evaluate (*pData) in expression panel instead):
while (hspi->TxXferCount > 0U)
{
/* Wait until TXE flag is set to send data */
if(__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXE))
{
*((__IO uint8_t*)&hspi->Instance->DR) = (*pData); //<--THIS LINE
pData += sizeof(uint8_t);
hspi->TxXferCount--;
}EDIT: Sorry my bad, TX line is wrong, updated.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.