2017-09-04 1:32 AM
Hi
In Software pack there is a 'stm32f407vgtx' micro and in legacy packs there is 'stm32f407vg'. I have a Discovery board that I bought about 4 years ago that has stm32f407vg micro on it. So Which one of these I must choose?
And the problem is here, when I choose stm32f407vg from legacy packs, it has no RTE page and I can't choose CMSIS files to add to my project!
2017-09-04 2:02 AM
The part numbering is documented in the datasheet for STM32F405xx_407xx (DocID022152 Rev 4) on page 170, and probably elsewhere.
V means the part has 100 pins,
G means it has 1024K of flash,
T means it is an LQFP package, and
x refers to the temperature range, e.g. 6 means -40 to 85 ^C.
Basically, the longer designation is just more specific about the physical nature of the part. I don't know that the numbering is case sensitive (there are no lower case alternatives for these particular parts), but recommend upper case as used by ST.
2017-09-07 12:40 AM
Thank you Alan,
So you say there is no difference between them?
Then why one micro has two definitions in 2 different pack(Software and legacy packs)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.