2008-04-01 8:17 PM
What need to change building a hex for IAP download?
2011-05-17 3:27 AM
STM32
the example boot code of IAP via UART takes up 8K byte , What need to change building a hex for IAP download? l, in lnkarm_flash.xcl ? // Code memory in FLASH -DROMSTART=0x8000000 ---> 0x8002000 ? -DROMEND=0x801FFFF 2, in NVIC_Configuration ? void NVIC_Configuration(void) { #ifdef VECT_TAB_RAM /* Set the Vector Table base location at 0x20000000 */ NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); #else /* VECT_TAB_FLASH */ /* Set the Vector Table base location at 0x08000000 */ NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); --->? #endif } 3, anything else?2011-05-17 3:27 AM
The STM32F10xxx in-application programming using the USART(AN 2575) shows how to generate a binary file(same thing for hex file). There is a pre-configured example under:
STM32F10x_IAP_AN/IAP_AN/binaryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.