2021-02-11 11:28 AM
Actually, i don't get any max value for UART baud rate in datasheet as well as in reference manual.
2021-02-11 11:55 AM
There is some info in en.STM32G4-Peripheral-USART_interface_USART.pdf. The issue with high baud rates is the baud rate precision that you can achieve with your given master clock and the BRR register settings. For 170 MHz and 8-fold oversampling the calculated max is 21,25 Mbaud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.