2019-12-19 7:24 PM
Hello,
In our custom board we are using STM32F429VG controller. Which has internal RAM of 256K.
I want to creating a screen with some animation using touchgfx designer. In that animation I want to create 3 circular rings each ring will contain 40 dots of a small circle image.
I have used array on image class as follows and used setXY, setBitmap to draw a circle.
Image imagering1[40];
Image imagering2[40];
Image imagering3[40];
But after code compilation I am getting error "unable to allocate space for sections/blocks with a total estimated minimum size of 0x3'027c bytes (max align 0x8) in <[0x2000'0000-0x2002'ffff]> (total uncommitted space 0x3'0000). " .
Board RAM utilization as follows
frameBuf0 0x2000'0048 0x25800 Data Lc BoardConfiguration.o [1]
dma 0x2002'e9dc 0x00aa0 Data Gb BoardConfiguration.o [1]
ucHeap 0x2002'5848 0x08000 Data Lc heap_4.o [1]
CSTACK 0x2002'f958 0x00400 <Block>
So I want to understand how Image Widget allocate memory. Is there any alternative way to create such animation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.