2023-06-07 7:18 PM
What is the difference between STM32L151CBU6 and STM32L151CBU6A?
Can they be interchangeably used?
2023-06-07 10:28 PM
Some year ago we tried to replace stm32l151rct6 by stm32l151rct6A.
We detected instability, may be due to pll default at startup.
We were surprised that A ref was very quickly NRFND (Not Recommanded For New Design).
May be it confirm that A ref was a bad try and was abandoned...
Now all stm32l1 are NRFND.
May be give a look to L4 or U5...
Not sure that it is pin to pin compatible for your design (you must check), but for sure that need rework for SW.
2023-06-07 10:55 PM
There is a technical note TN1176 describing the migration from e.g. the (older) STM32L15xx6/8/B to the (newer) STM32L15xx6/8/B-A and the differences.
Yes, both are already on NRND, but will still be produced until the end of 2031. Nevertheless, as @GLASS noted, it makes sense to switch to another family.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.