2021-02-17 6:45 PM
This is the sequence of events:
2021-02-18 1:36 PM
Which 'L4 exactly? Is this some "known good" hardware like Nucleo/Disco? Is there any battery/capacitor on VBAT? Is the supply removal complete (VDD shoes hard to ground)? Is the power supply voltage high enough and stable during second wake-up? Is the behaviour different without the brownout?
JW
2021-02-18 1:41 PM
I'm seeing this on STM32L475VGT and STM32L475VET. I've demonstrated the issue on the B-L475E-IOT01A Discovery kit as well as my own hardware. Powered by battery or a power supply.
2021-02-19 12:24 AM
Is the behaviour different without the brownout?
JW
2021-02-19 8:02 AM
Yes, for example if you give a low going pulse on the NRST pin, you get the PINRST flag for the corresponding wake/reset. The following wake the flag is cleared as it should be.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.