2014-10-22 12:51 AM
used for many years
Keil
products
,
but
lately
I find
that it contains
more errors
,
backlogs
and
problems than
is healthy.
Is there
TrueStudio
or
IAR
Embedded
Workbench
for
ARM
better
?
2014-10-22 2:32 AM
Hi
You are going to cause a flame war here ! ''used for many years
Keil
products
,
but
lately
I find
that it contains
more errors
,
backlogs
and
problems than
is healthy.
'' I have not used it now for many years but that is the impression I get from some of the other poster here. ''Is there
TrueStudio
or
IAR
Embedded
Workbench
for
ARM
better
?
'' I am forced to use Atollic TrueStudio here at work and I hate it with a passion! Probably, the worst problem (for embedded developers) is the problem of confidence in the debugger : sometimes in Atollic you press single step and the debugger does not come back to the next line for a LONG (we are talking minutes here) time. The rep reckons it is the ST-Link debugger. I suspect it is the Eclipse underneath doing some kind of a project inspection under the hood. Not to mention that fact that even though I have configured Atollic/Eclipse to insert spaces instead of Tabs - it still inserts Tabs Do not even get me started about the whole 'Tabbed window' thing. Do NOT recommend Atollic - avoid if you can. I used IAR at my last company. The Editor is not that great, lots it could do better. The Debugger - does what it says on the tin. Very reliable debugger (used Segger JTag at work, seems OK with the ST-Link but only played with ST-Link and IAR at home). I do like IAR. (That is my personal and professional opinion)2014-10-22 5:19 AM
Enquiry
I
thought
seriously.
Depending on your
answers
,
it seems
,
everything
is the same
misery
.Due to
BT
stack for
CC2540
I
used a
little
IAR
for
8051
and
not particularly
impressed
.
Atollic
I did not know
,
so I was hoping
for a miracle.
Well,
thank you
for
returning
to
reality
2014-10-22 6:09 AM
You should perhaps be a little more specific about your needs and intentions.
There are several toolchains/IDEs which are quite useful for hobbyists, but not really ready for professional use. CoIDE, EmBlocks and Yagarto are amongst them. As professional, you are usually not free to put the look&feel of the IDE over hard facts like code size, user support, debug support, integration of test frameworks, version management etc.2014-10-22 6:21 AM
''You are going to cause a flame war here !''
''Enquiry
I
thought
seriously.
'' My comment was not meant as a personal insult - just be careful about what and how you ask. ''What is the best IDE for STM32 ?'' will illicit all kinds of personal views! Then people will start arguing about it. ''it seems
,
everything
is the same
misery
.'' As I said, I prefer IAR because the debugging side give me confidence in what the debugger and my code is doing. Did not notice IAR bugs or crashes when I last used it. Atollic has all kinds of issues, which is to do with Eclipse. It has also crashed on me but not very often. As FM has said - you have not specified what you will be using this for hobbyist or professional use. Personally, Atollic has put me off Eclipse so much that I will avoid anything that is built on Eclipse. I had the miss-fortune to use Freescale's Codewarrier (also built on top of Eclipse) on one of their training semiars. Had the same problems as Atollic - slow, clumsy and does not give you confidence in the debugging. One more thing that Eclipse handles really badly is the 'Porject' concept, it just does not know the difference between directories and a project. It mixes the 2 up so badly that I cannot work on the same project in multiple directories, something that IAR and VisualStudio does so easily. Therefore I would not even look at CoIDE (aka CooCox ) because it too is a Eclipse customisation. I have not tried emBlocks yet.2014-10-22 7:10 AM
It might be a serious question, but it's entirely subjective, as ''best'' means different things to different people. Thus you'll get a flame war.
I also really dislike Eclipse based tools, the evaluation of Atollic was painful, and honestly I can use Eclipse and GNU/GCC without paying someone. Choices are usually driven be personal preference, and corporate edict.2014-10-22 7:15 AM
One more thing that Eclipse handles really badly is the 'Porject' concept, it just does not know the difference between directories and a project. It mixes the 2 up so badly that I cannot work on the same project in multiple directories, something that IAR and VisualStudio does so easily.
Totally this - the whole project/workspace thing is a complete cluster.2014-10-22 10:28 AM
Totally this - the whole project/workspace thing is a complete cluster.
I had been told that this concept of workspace / virtual project folders allows for easy multi-project development and debugging. But being accustomised to a filesystem-based project structure, that Eclipse idea is totally lost on me, too. In addition, important features like project import, file import and debug setup are counter-intuitive and totally messed up.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.