2018-10-11 2:49 PM
DS12110 Rev 5, notes for Figure 40. says it should be in Table 85 but it isn't. Rain and Cadc are in the Table 85.
2018-11-06 8:02 AM
Hello all,
Would also like to know the answer to this one.
Anyone any idea??
Regards,
2019-04-16 1:50 PM
I suspect it may differ for fast versus slow channels. I would also like to know.
2019-04-17 1:27 PM
I got a reply from ST in a support ticket. Their recommendation is to use table 185 in the datasheet (it’s in the revision V section, but the rep said it applies to revision Y as well).
2019-04-18 10:24 AM
The Rev 6 datasheet still calls out Radc in two places and says look for it in two tables. This note should be removed if Radc isn't going to be provided.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.