2021-10-22 2:01 AM
Several MCU are described with the label 'value line' but I could not find an explanation what that mean. I assume it is related to a system architecture, right?
Solved! Go to Solution.
2021-10-22 2:20 AM
With the Value line, individual functions were measured with looser tolerances or were completely omitted for reasons of cost. If you compare the data sheets of the Value Line with those of the Access Line, you can see very quickly which parameters are affected. Sometimes it is the voltage range, sometimes the missing serial number, or other parameters.
Regards
/Peter
2021-10-22 2:20 AM
With the Value line, individual functions were measured with looser tolerances or were completely omitted for reasons of cost. If you compare the data sheets of the Value Line with those of the Access Line, you can see very quickly which parameters are affected. Sometimes it is the voltage range, sometimes the missing serial number, or other parameters.
Regards
/Peter
2021-10-22 2:37 AM
Thank you very much for the fast answer.
Led
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.