2014-06-18 7:54 PM
I want to change to TIM9_CH1 point to PE5 in STM32Cube_FW_F4_V1.1.0\Projects\STM324x9I_EVAL\Examples\TIM\TIM_PWMOutput. The main.h is:
~~~~~~~~~~ #define TIMx TIM3 #define TIMx_CLK_ENABLE __TIM3_CLK_ENABLE /* Definition for USARTx Pins */ #define TIMx_CHANNEL_GPIO_PORT() __GPIOC_CLK_ENABLE() #define GPIO_PIN_CHANNEL1 GPIO_PIN_6 #define GPIO_PIN_CHANNEL2 GPIO_PIN_7 #define GPIO_PIN_CHANNEL3 GPIO_PIN_8 #define GPIO_PIN_CHANNEL4 GPIO_PIN_9 ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ I change it to: ~~~~~~~~~~~~~~~~~~~~~~~~~~ #define TIMx TIM9 #define TIMx_CLK_ENABLE __TIM9_CLK_ENABLE /* Definition for USARTx Pins */ #define TIMx_CHANNEL_GPIO_PORT() __GPIOE_CLK_ENABLE() #define GPIO_PIN_CHANNEL1 GPIO_PIN_5 #define GPIO_PIN_CHANNEL2 GPIO_PIN_7 #define GPIO_PIN_CHANNEL3 GPIO_PIN_8 #define GPIO_PIN_CHANNEL4 GPIO_PIN_9 ~~~~~~~~~~~~~~~~~~~~~ But it doesn't work. Please help. Thanks2014-06-20 3:09 AM
Please help, why it can not be pointed to other port?
2014-06-20 6:15 AM
Probably because there are other dependencies within the code tree that these defines don't address. You're going to need to learn to walk through the code to understand it.
STM32Cube_FW_F4_V1.0.0\Projects\STM324x9I_EVAL\Examples\TIM\TIM_PWMOutput\Src\stm32f4xx_hal_msp.c Makes specific reference to GPIOC when initializing the pins, and TIM3void HAL_TIM_PWM_MspInit(TIM_HandleTypeDef *htim)
{
GPIO_InitTypeDef GPIO_InitStruct;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* TIMx Peripheral clock enable */
TIMx_CLK_ENABLE();
/* Enable GPIO Channels Clock */
TIMx_CHANNEL_GPIO_PORT();
/*##-2- Configure I/Os #####################################################*/
/* Configure PC.6 (TIM3_Channel1), PC.7 (TIM3_Channel2), PC.8 (TIM3_Channel3),
PC.9 (TIM3_Channel4) in output, push-pull, alternate function mode
*/
/* Common configuration for all channels */
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF2_TIM3;
GPIO_InitStruct.Pin = GPIO_PIN_CHANNEL1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_CHANNEL2;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_CHANNEL3;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_CHANNEL4;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
}
Your life might also be a lot easier if you use the Standard Library rather than the HAL/CUBE thing.
2014-06-20 6:20 AM
Another possibility - PE 7, 8, and 9 are not TIM9 channels.
Cheers, Hal2014-06-20 10:21 AM
Another possibility - PE 7, 8, and 9 are not TIM9 channels.
It only has two channels, but the question really seems to be about CH1 These kinds of half-assed examples, here and in the standard library do annoy me. It's like look here I have these defines to abstract the pins/peripheral on some hardware platforms, but then it breaks because the abstraction is incomplete, or there is some assumption about APB1 or APB2 that's hard coded deeper in the configuration routine.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.