2014-11-03 1:14 AM
I work with the Wakeup pin (PA0) as STandBy wakeup.
When I set PA0=''0'' change it to WakeUP pin and then enter StandBy. When I make PA0=''1'' it get out of the Standby state and work as usuall.But when I enter to StandBy after confige it and PA0=''1'' and then try to toggle PA0 ->0->1 it doesn't work.I do all the glage clear before enter Standby.Here is the code for entering Standby: PWR_WakeUpPinCmd(ENABLE); //Enables the WakeUp Pin functionality /* Clear Wakeup flag */ PWR->CR |= PWR_CR_CWUF; /* Clear all RTC flages that can mask the WUF function */ RTC_ClearFlag(RTC_FLAG_ALRBF | RTC_FLAG_ALRAF | RTC_FLAG_TSF | RTC_FLAG_WUTF| RTC_FLAG_TAMP1F ); /* Request to enter STANDBY mode */ PWR_EnterSTANDBYMode(); // enter to StandBy mode As I read it the Wakeup work on rise enge and not level.DO I miss soemthing?Bar. #wakeup-pin-standby-stm32f2052014-11-03 1:27 AM
Read the manual.
RM0033, ''Exiting Standby mode'': ''The microcontroller exits Standby mode [...] a rising edge on WKUP pin [...]'' JW2014-11-03 3:41 AM
2014-11-03 4:09 AM
How do you set PA0 to 1, by applying an external voltage?
Could help? JW2014-11-03 11:51 PM
I look on that thread.
I do as ST propose to get over the PA0=''1'' when go to Standby.1. Make WakeUp function, disable.2. Clear the Wakeup flag.3. Clear all RTC flages also.3. Enable Wakeup function.4. Enter StandBy.Don't get out of StandBy when go 1->0->1.Any idea?Bar.2014-11-04 12:19 AM
Can you please post a minimal but complete compilable code which exhibits the problem?
JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.