2010-06-21 8:30 AM
W5100 Ethernet Chip SPI code
2011-05-17 4:55 AM
''it doesn't go very well''
What, exactly, do you mean by that?2011-05-17 4:55 AM
I doesn't get any sign of life from it...
So maybe the SPI isn't set up properly or maybe it's just me that haven't ported it correctly.
I've uploaded the code - keep in mind that it is a mix of my fully working LCD library/interface which I use for debugging, and the not working ported W5100 code!
Download it here: http://elec.tkjweb.dk/SSD1963_W5100.zip
Best Regards
Thomas Jespersen
2011-05-17 4:55 AM
''I doesn't get any sign of life from it... So maybe the SPI isn't set up properly''
Have you checked with a scope that the clock is being generated? And any required chip select? And data on the data lines?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.