2012-07-11 10:09 PM
hi,
i search and search but i cant find where i can change Vector Table base location in memory.map i can find .text 0x08004000 0x718 *(.isr_vector .isr_vector.*) .isr_vector 0x08004000 0x124 ..\obj\startup_stm32f10x_md_vl.o 0x08004000 g_pfnVectors *(.text .text.* .gnu.linkonce.t.*) in memory.ld rom (rx) : ORIGIN = 0x08004000, LENGTH = 0x00002000 but i need to change vector table address to 0x08000000 NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x08000000); - this isnt working ..... i am using stm32f100 and coocox ide ....2015-09-11 12:20 PM
2015-09-11 4:41 PM
Not familiar with your compiler/assembler. The vector table, as used by the M0, has TWO entries in the front portion. The initial Stack Pointer, which should point into a higher area of RAM, and the initial Program Counter (aka ResetHandler function)
+0 SP+4 PC+8 NMI Handler+12 Hard Fault Handler...2015-10-10 1:43 PM
Thanks, Clive,
Sorry about late reply. Thanks for valuable STM32 insight (not just this post... MANY of your posts are VERY helpful.) I'm using the ImageCraft (Palo Alto, CA) ICC/Jumpstart ARM C compiler for STM32F0xxx parts; The ICC compiler supports a bunch of different STM 32 ARM devices. For some reason, the SP pointer was not described... I guess for obv. reasons. (i.e. keep me away from producing a BRICK!) I find that the Imagecraft ICC compiler was free (~30 days/ 64KB, etc.) and it was easy to use, so ended up purchasing a license ($99.USD) and it performs really fast (~5K lines+ in ~3 or 4 seconds.) I had used the ICC compiler many years ago for a Motorola uC, so I was slightly familiar with their old (ancient) compilers. Oh, and a single menu selection downloads the code to the USB-connected device... I can change lines, re-comp and re-upload in less-than ~30 seconds (64KB.) At first, I tried GCC (SLOWWWW Compile!!!! And, LONG TIME TO INSTALL!!!!) Plus the amount of crappo GCC place onto my laptop was astounding! Also, I tried the ST Cloud solution: Very robust, very complete! Very nice cloud solution ... but very hard to perform rapid prototyping. I like to fix, test, test, test, fix... Sometimes re-compile each minute until solution works. So, I needed a quick compiler solution. I suspect that in future, the cloud will be the ONLY way to compile. (Imagine a cloud supercomputer compiling your code [and everyone else's] ....) Regarding the ICC Compiler: The most important thing I find, is that the installation time is minutes. Plus, I like to cycle test rapidly during prototyping. Some of the other compilers I looked at cost too much $$$. The Imagecraft compiler is the right price and super performance. ImageCraft are a small company, so when you ask for help, you get the CEO or one of the few developers. This helps a lot. If you get a chance, you should consider trying the ImageCraft compiler. (BTW: I loved your reply concerning ADC and DMA! Very good work. Thanks!] -Chris p.s. I do not have any relationship with ICC except that I bought their compiler license.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.