2019-02-27 3:48 PM
RM0038 Reference manual
STM32L100xx, STM32L151xx, STM32L152xx and STM32L162xx advanced ARM®-based 32-bit MCUs
Figure 8. Power supply overview
(LQFTP100)
has the following note:
If I am using separate supply for VDDA should I still connect them?
Table 58. ADC pins
has the following:
2.4 V ≤ VDDA ≤ VDD (3.6 V) for full speed
It means VDDA can be less than VDD.
Manual is a bit confusing. Please help! Which one is a correct statement:
Solved! Go to Solution.
2019-02-28 3:36 PM
No problem! thanks for the help! I couldn't find anything about tying VDDA and VDD in STM32L4 data sheet. Though it has fewer ADCs.
Might need to reduce ADC speed so I can use VREF+ = 2.5V and VDDA = 3.3V.
Still don't understand why do we need VDDA pin if it is going to be tied to VDD. Oh well.
2019-08-04 2:01 AM
VDDA could be derived using a low noise LDO from VDD
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.