2017-11-13 6:04 AM
Hello all,
Using
STM32L1XX_NUCLEO
with
F_CPU
equal to
32
MHz
,
the
RTIMER_ARCH_SECOND
is
defined as
32768 in the file platform-conf.h.
Please,
what are
the value
s
of
RTIMER_ARCH_SECOND
for frequenc
ies
rather than 32MHz,
such as;
24MHz, 16MHz and 12MHz?
M
any thanks for your time and look forward for your response.
B
est regards,
Wassim
2017-11-13 6:32 AM
32768
seems related to the RTC quarz.2017-11-13 6:58 AM
It's really a Contiki OS thing, are you sure they are even directly related? Or just a fractional representation of another clock?
2017-11-13 7:18 AM
As seen in the following link, the RTIMER_ARCH_SECOND is given by F_CPU/RTIMER_ARCH_PRESCALER, where RTIMER_ARCH_PRESCALER is eqaul to 1024.
http://contiki.sourceforge.net/docs/2.6/a00792_source.html
However, in the file /Middlewares/ST/Contiki_STM32_Library/Incplatform-conf.h, RTIMER_ARCH_SECOND is defined as: #define RTIMER_ARCH_SECOND 32768 for STM32L1XX_NUCLEO using F_CPU=32MHz and defined as: #define RTIMER_ARCH_SECOND 96000 for STM32F4XX_NUCLEO using F_CPU=84MHz. Hence, I am not sure if they are directly related or not.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.