2018-04-05 6:21 AM
Hi
I am about to choose a STM32L4 chip and want to use the VREFBUF for more accurate readings, and seems to be as accurate as external reference chips. I havent used this before and couldnt find the answer when searching on the forum. What I am not sure about is if this is simply an output that has to be tied to the VREF+ input pin? Or after its enabled , then internal circuit uses it, saving the need to connect to external VREF+ input pin?
Many Thanks
Scott
2018-04-05 11:58 AM
IMO the description in the Voltage reference buffer (VREFBUF) chapter of RM is clear in this - it connects internally to the VREF+ pin.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.