2018-09-06 10:17 PM
I have an LCD is on an 8080 16bit FMC interface with A0 register select.
I can read the status correctly here:
#define LCD1_DEVICE_ADDR (uint32_t)0x60000000
#define LCD1_DEVICE_DATA (uint32_t)0x60000001
uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR;
readLcdStatus = *pLcdRStatusWAddress;
All of these snippets are within one file,
//this compiles:
inline lcdRegDataWrite(uint8_t reg, uint8_t data) {
*(__IO uint16_t*)LCD1_DEVICE_ADDR = reg;
*(__IO uint16_t*)LCD1_DEVICE_DATA = data;
}
//but this doesn't find it
lcdRegDataWrite( 1 , 8);
>>> undefined reference to `lcdRegDataWrite'
2018-09-12 5:33 AM
Hi @Community member ,
Could you please provide more details on your case: which compiler? which device? is this your own code or found in an example provided by ST?...
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-09-12 5:49 AM
Check with your compiler vendor, review example others are using and that work
2018-09-13 6:48 AM
this is the full compiler output...
1>------ Build started: Project: TH218_sln, Configuration: Debug Win32 ------
1>VisualGDB: Run "C:\SysGCC\arm-eabi\bin\make.exe CONFIG=Debug -j4" in directory "C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln" on local computer
1>C:/SysGCC/arm-eabi/bin/arm-eabi-gcc.exe -ggdb -ffunction-sections -O0 -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -IC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.mbed/cmsis/TARGET_CORTEX_M -I..\..\TH218\Inc -I..\..\TH218\Drivers\CMSIS\Device\ST\STM32H7xx\Include -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Core\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc\Legacy -I..\..\TH218\Middlewares\Third_Party\FatFs\src -I. -DDEBUG=1 -Dflash_layout -DSTM32H753xx -DARM_MATH_CM7 -DSTM32H753BI -c ../../TH218/Lefty/lcd.c -o Debug/lcd.o -MD -MF Debug/lcd.dep
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(2):
1>../../TH218/Lefty/lcd.c: In function 'initRa8877Pins':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
1> ^
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(65,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
1> ^~~~~~~~~~~~~~~~
1>../../TH218/Lefty/lcd.c: In function 'initRA8877':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
1> ^
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(84,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
1> ^~~~~~~~~~~~~~~~
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(14,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
1> #define LCD1_DEVICE_DATA (uint32_t)0x60000001
1> ^
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(87,26): note : in expansion of macro 'LCD1_DEVICE_DATA'
1> uint16_t *pLcdData = LCD1_DEVICE_DATA;
1> ^~~~~~~~~~~~~~~~
1>C:/SysGCC/arm-eabi/bin/arm-eabi-g++.exe -o Debug/TH218_sln.elf -Wl,-gc-sections --specs=nano.specs --specs=nosys.specs -TC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32H7xxxx/LinkerScripts/STM32H753BI_flash.lds -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wl,--start-group Debug/bios.o Debug/lcd.o Debug/sdram.o Debug/Ra8876_Lite.o Debug/usb_device.o Debug/usbd_conf.o Debug/usbd_desc.o Debug/usbd_cdc_if.o Debug/stm32h7xx_it.o Debug/stm32h7xx_hal_msp.o Debug/stm32h7xx_hal_timebase_TIM.o Debug/main.o Debug/system_stm32h7xx.o Debug/stm32h7xx_hal.o Debug/stm32h7xx_hal_adc.o Debug/stm32h7xx_hal_adc_ex.o Debug/stm32h7xx_hal_rtc.o Debug/stm32h7xx_hal_rtc_ex.o Debug/stm32h7xx_hal_fdcan.o Debug/stm32h7xx_hal_rng.o Debug/stm32h7xx_ll_fmc.o Debug/stm32h7xx_hal_nand.o Debug/stm32h7xx_hal_spi.o Debug/stm32h7xx_hal_spi_ex.o Debug/stm32h7xx_hal_mdma.o Debug/stm32h7xx_ll_sdmmc.o Debug/stm32h7xx_hal_sd.o Debug/stm32h7xx_hal_sd_ex.o Debug/stm32h7xx_hal_hsem.o Debug/stm32h7xx_hal_cortex.o Debug/stm32h7xx_hal_cryp.o Debug/stm32h7xx_hal_cryp_ex.o Debug/stm32h7xx_hal_dma.o Debug/stm32h7xx_hal_dma_ex.o Debug/stm32h7xx_hal_i2c.o Debug/stm32h7xx_hal_i2c_ex.o Debug/usbd_core.o Debug/usbd_ctlreq.o Debug/usbd_ioreq.o Debug/usbd_cdc.o Debug/stm32h7xx_hal_spdifrx.o Debug/stm32h7xx_hal_uart.o Debug/stm32h7xx_hal_uart_ex.o Debug/stm32h7xx_hal_pwr.o Debug/stm32h7xx_hal_pwr_ex.o Debug/stm32h7xx_hal_sram.o Debug/stm32h7xx_hal_flash.o Debug/stm32h7xx_hal_flash_ex.o Debug/stm32h7xx_hal_gpio.o Debug/stm32h7xx_hal_hash.o Debug/stm32h7xx_hal_hash_ex.o Debug/stm32h7xx_hal_pcd.o Debug/stm32h7xx_hal_pcd_ex.o Debug/stm32h7xx_ll_usb.o Debug/stm32h7xx_hal_hrtim.o Debug/stm32h7xx_hal_rcc.o Debug/stm32h7xx_hal_rcc_ex.o Debug/stm32h7xx_hal_crc.o Debug/stm32h7xx_hal_crc_ex.o Debug/stm32h7xx_hal_eth.o Debug/stm32h7xx_hal_tim.o Debug/stm32h7xx_hal_tim_ex.o Debug/stm32h7xx_hal_sai.o Debug/stm32h7xx_hal_sai_ex.o Debug/stm32h7xx_hal_sdram.o Debug/stm32h7xx_hal_qspi.o Debug/startup_stm32h753xx.o Debug/bsp_driver_sdram.o Debug/sdram_diskio.o Debug/fatfs.o Debug/diskio.o Debug/ff.o Debug/ff_gen_drv.o Debug/syscall.o -Wl,--end-group
1>Debug/lcd.o: In function `initRA8877':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(95): error : undefined reference to `lcdRegDataWriten'
1>collect2.exe : error : ld returned 1 exit status
1>make: *** [Debug/TH218_sln.elf] Error 1
1>-------------------------------------------------------------
1>Command exited with code 2
1>Executable: C:\SysGCC\arm-eabi\bin\make.exe
1>Arguments: CONFIG=Debug -j4
1>Directory: C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln
1>VisualGDB : error : Command-line action failed
1>C:\Program Files (x86)\Microsoft Visual Studio\2017\Community\Common7\IDE\VC\VCTargets\Microsoft.MakeFile.Targets(44,5): error MSB3073: The command ""C:\Program Files (x86)\Sysprogs\VisualGDB\\VisualGDB.exe" /build "C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\TH218_sln.vcxproj" "/solution:C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln.sln" "/config:Debug" "/platform:Win32"" exited with code 1.
1>Done building project "TH218_sln.vcxproj" -- FAILED.
========== Build: 0 succeeded, 1 failed, 0 up-to-date, 0 skipped ==========
2018-09-13 6:55 AM
The extra 'n' at the end of
lcdRegDataWriten
?
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(95): error : undefined reference to `lcdRegDataWriten'
JW
2018-09-13 7:00 AM
Yes, I renamed it for the forum, .. well spotted..
I added the Void but that didn't help.
inline void lcdRegDataWriten(char reg, char data) {
// *(__IO uint16_t*)LCD1_DEVICE_ADDR = reg;
// *(__IO uint16_t*)LCD1_DEVICE_DATA = data;
*(__IO uint16_t*)0x60000000 = reg;
*(__IO uint16_t*)0x60000001 = data;
}
2018-09-13 8:48 AM
Okay so post the whole offending file which caused the output above, or post the file together with the output, so we have a complete view.
Also, try to add a line
#error "no compile"
just below the line
inline void lcdRegDataWriten(char reg, char data) {
JW
2018-09-18 9:04 PM
thanks for the pointers @Community member, @Community member
was this the output you expected ?
1>------ Build started: Project: TH218_sln, Configuration: Debug Win32 ------
1>VisualGDB: Run "C:\SysGCC\arm-eabi\bin\make.exe CONFIG=Debug -j4" in directory "VS2018\TH218_sln\TH218_sln" on local computer
1>C:/SysGCC/arm-eabi/bin/arm-eabi-gcc.exe -ggdb -ffunction-sections -O0 -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -IC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.mbed/cmsis/TARGET_CORTEX_M -I..\..\TH218\Inc -I..\..\TH218\Drivers\CMSIS\Device\ST\STM32H7xx\Include -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Core\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc\Legacy -I..\..\TH218\Middlewares\Third_Party\FatFs\src -I. -DDEBUG=1 -Dflash_layout -DSTM32H753xx -DARM_MATH_CM7 -DSTM32H753BI -c ../../TH218/Lefty/lcd.c -o Debug/lcd.o -MD -MF Debug/lcd.dep
1>../../TH218/Lefty/lcd.c: In function 'lcdRegDataWriten':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(16,2): error : #error "no compile"
1> #error "no compile"and this is the current code:
inline void lcdRegDataWriten(char reg, char data) {
#error "no compile"
// *(__IO uint16_t*)LCD1_DEVICE_ADDR = reg;
// *(__IO uint16_t*)LCD1_DEVICE_DATA = data;
*(__IO uint16_t*)0x60000000 = reg;
*(__IO uint16_t*)0x60000001 = data;
} this is the usage:
lcdRegDataWriten(1, 8);
with #error compile removed:
1>------ Build started: Project: TH218_sln, Configuration: Debug Win32 ------
1>VisualGDB: Run "C:\SysGCC\arm-eabi\bin\make.exe CONFIG=Debug -j4" in directory "C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln" on local computer
1>C:/SysGCC/arm-eabi/bin/arm-eabi-gcc.exe -ggdb -ffunction-sections -O0 -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -IC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.mbed/cmsis/TARGET_CORTEX_M -I..\..\TH218\Inc -I..\..\TH218\Drivers\CMSIS\Device\ST\STM32H7xx\Include -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Core\Inc -I..\..\TH218\Middlewares\ST\STM32_USB_Device_Library\Class\CDC\Inc -I..\..\TH218\Drivers\STM32H7xx_HAL_Driver\Inc\Legacy -I..\..\TH218\Middlewares\Third_Party\FatFs\src -I. -DDEBUG=1 -Dflash_layout -DSTM32H753xx -DARM_MATH_CM7 -DSTM32H753BI -c ../../TH218/Lefty/lcd.c -o Debug/lcd.o -MD -MF Debug/lcd.dep
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(2):
1>../../TH218/Lefty/lcd.c: In function 'initRa8877Pins':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
1> ^
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(64,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
1> ^~~~~~~~~~~~~~~~
1>../../TH218/Lefty/lcd.c: In function 'initRA8877':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(13,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
1> #define LCD1_DEVICE_ADDR (uint32_t)0x60000000
1> ^
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(83,37): note : in expansion of macro 'LCD1_DEVICE_ADDR'
1> uint16_t *pLcdRStatusWAddress = LCD1_DEVICE_ADDR; // read status or write address
1> ^~~~~~~~~~~~~~~~
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\bios.h(14,27): warning : initialization makes pointer from integer without a cast [-Wint-conversion]
1> #define LCD1_DEVICE_DATA (uint32_t)0x60000001
1> ^
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(86,26): note : in expansion of macro 'LCD1_DEVICE_DATA'
1> uint16_t *pLcdData = LCD1_DEVICE_DATA;
1> ^~~~~~~~~~~~~~~~
1>C:/SysGCC/arm-eabi/bin/arm-eabi-g++.exe -o Debug/TH218_sln.elf -Wl,-gc-sections --specs=nano.specs --specs=nosys.specs -TC:/Users/nickm/AppData/Local/VisualGDB/EmbeddedBSPs/arm-eabi/com.sysprogs.arm.stm32/STM32H7xxxx/LinkerScripts/STM32H753BI_flash.lds -mcpu=cortex-m7 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -Wl,--start-group Debug/bios.o Debug/lcd.o Debug/sdram.o Debug/Ra8876_Lite.o Debug/usb_device.o Debug/usbd_conf.o Debug/usbd_desc.o Debug/usbd_cdc_if.o Debug/stm32h7xx_it.o Debug/stm32h7xx_hal_msp.o Debug/stm32h7xx_hal_timebase_TIM.o Debug/main.o Debug/system_stm32h7xx.o Debug/stm32h7xx_hal.o Debug/stm32h7xx_hal_adc.o Debug/stm32h7xx_hal_adc_ex.o Debug/stm32h7xx_hal_rtc.o Debug/stm32h7xx_hal_rtc_ex.o Debug/stm32h7xx_hal_fdcan.o Debug/stm32h7xx_hal_rng.o Debug/stm32h7xx_ll_fmc.o Debug/stm32h7xx_hal_nand.o Debug/stm32h7xx_hal_spi.o Debug/stm32h7xx_hal_spi_ex.o Debug/stm32h7xx_hal_mdma.o Debug/stm32h7xx_ll_sdmmc.o Debug/stm32h7xx_hal_sd.o Debug/stm32h7xx_hal_sd_ex.o Debug/stm32h7xx_hal_hsem.o Debug/stm32h7xx_hal_cortex.o Debug/stm32h7xx_hal_cryp.o Debug/stm32h7xx_hal_cryp_ex.o Debug/stm32h7xx_hal_dma.o Debug/stm32h7xx_hal_dma_ex.o Debug/stm32h7xx_hal_i2c.o Debug/stm32h7xx_hal_i2c_ex.o Debug/usbd_core.o Debug/usbd_ctlreq.o Debug/usbd_ioreq.o Debug/usbd_cdc.o Debug/stm32h7xx_hal_spdifrx.o Debug/stm32h7xx_hal_uart.o Debug/stm32h7xx_hal_uart_ex.o Debug/stm32h7xx_hal_pwr.o Debug/stm32h7xx_hal_pwr_ex.o Debug/stm32h7xx_hal_sram.o Debug/stm32h7xx_hal_flash.o Debug/stm32h7xx_hal_flash_ex.o Debug/stm32h7xx_hal_gpio.o Debug/stm32h7xx_hal_hash.o Debug/stm32h7xx_hal_hash_ex.o Debug/stm32h7xx_hal_pcd.o Debug/stm32h7xx_hal_pcd_ex.o Debug/stm32h7xx_ll_usb.o Debug/stm32h7xx_hal_hrtim.o Debug/stm32h7xx_hal_rcc.o Debug/stm32h7xx_hal_rcc_ex.o Debug/stm32h7xx_hal_crc.o Debug/stm32h7xx_hal_crc_ex.o Debug/stm32h7xx_hal_eth.o Debug/stm32h7xx_hal_tim.o Debug/stm32h7xx_hal_tim_ex.o Debug/stm32h7xx_hal_sai.o Debug/stm32h7xx_hal_sai_ex.o Debug/stm32h7xx_hal_sdram.o Debug/stm32h7xx_hal_qspi.o Debug/startup_stm32h753xx.o Debug/bsp_driver_sdram.o Debug/sdram_diskio.o Debug/fatfs.o Debug/diskio.o Debug/ff.o Debug/ff_gen_drv.o Debug/syscall.o -Wl,--end-group
1>Debug/lcd.o: In function `initRA8877':
1>C:\Users\nickm\Documents\VS2018\TH218_sln\TH218_sln\..\..\TH218\Lefty\lcd.c(94): error : undefined reference to `lcdRegDataWriten'
1>collect2.exe : error : ld returned 1 exit status
1>make: *** [Debug/TH218_sln.elf] Error 1sorry for the delayed response
2018-09-18 11:06 PM
Post the sources, possibly reduced to a bare minimum which still compiles and produces the problem.
JW
2018-09-19 12:19 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.