2014-09-16 4:54 AM
I am trying to use multiple interupts on my nucleo board. I have used the cube hal. My problem is that I dont get the interrupts generated on the PB0 pin, but the PB1 works ok.
I have tried to do the intialization in different order and it seems like it works better, but I dont understand why the HAL needs calls in a specific order. My code to initialize the interrupts are based on the GPIO_EXTI example:static void EXTI_Config(void)
{ GPIO_InitTypeDef GPIO_InitStructure; /* Enable GPIOB clock */ __GPIOB_CLK_ENABLE(); /* Configure PB0 pin */ GPIO_InitStructure.Mode = GPIO_MODE_IT_FALLING; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Pin = GPIO_PIN_0; GPIO_InitStructure.Speed = GPIO_SPEED_FAST; HAL_GPIO_Init(GPIOB, &GPIO_InitStructure); /* Configure PB1 pin */ GPIO_InitStructure.Mode = GPIO_MODE_IT_FALLING; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Pin = GPIO_PIN_1; GPIO_InitStructure.Speed = GPIO_SPEED_FAST; HAL_GPIO_Init(GPIOB, &GPIO_InitStructure); /* Enable and set EXTI Interrupt to the lowest priority */ HAL_NVIC_SetPriority(EXTI0_1_IRQn, 3, 0); HAL_NVIC_EnableIRQ(EXTI0_1_IRQn); }2014-09-18 3:39 AM
Hello Johan,
Could you please let us know what was the working sequence & the non-working one? Thanks -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-09-18 8:52 AM
Hihedlund.johan,
Please find attached a GPIO_EXTI project using mutliple GPIO interrupts on PB0 and PB1 with the STM32L053 Nucleo board and the STM32Cube_FW_L0_V1.1.0 package availablehttp://www.st.com/web/en/catalog/tools/PF260508#
. Let's try with this and keep us informed with your finding. # Please extract atSTM32Cube_FW_L0_V1.1.0\Firmware\Projects\STM32L053R8-Nucleo\Examples\GPIO Cheers, Heisenberg. ________________ Attachments : GPIO_EXTI_MUL.7z : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzZR&d=%2Fa%2F0X0000000bNh%2FK6hlu6yoDNmIu_rpjdKI1xQ21dB6IAR1hsuJedxK7E8&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.