2026-03-03 12:12 PM - last edited on 2026-03-13 5:21 AM by Amel NASRI
Greetings,
I am working with the STM32U585RI and a sensor that asserts an interrupt on the MISO line. I would like to know whether this setup is feasible, and if so, how best to implement it.
One approach I have considered is to use a separate pin (LPGPIO) to monitor the interrupt condition and then trigger the SPI sequence. However, during ongoing SPI transactions, I would need to temporarily disable the interrupt feature and re‑enable it after each transaction.
My question is, how can this be achieved using LPBAM? Is there a recommended way to configure LPBAM so that the interrupt handling and SPI transfers can coexist without conflict? Any suggestions or guidance would be greatly appreciated.
Best regards,
Rasool
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.