2013-02-23 5:29 PM
Hello everyone.
As many may have noticed, the STM32F4 discovery boards comes with an unfitted OSC32 crystal (X3) & biasing caps (C16 & C27). Did anyone ever tried to provide her/his the board with those missing components. I tried to solder a 32.768Hz T6 crystal, salvage from a functionnal digital clock, along with 15pF caps, but no matter what, the LSERY flag never get set even though LSEON is. Of course, I didn't provide VBAT any external supply, since it's bridged to VDD through R26, but the LSE is bound to be powered by VDD due to the internal reset circuitry anyway. Still, no oscillation on the crystal's pins... strange. Did I neglect some hardware configuration ? #stm32f4discovery-rtc-lse-crystal2013-07-02 1:13 PM
Thank you clive1, you are 90% of manpower on this forum!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.